Industrial camera IDS NXT malibu with lens and connected cable

Series launch: First industrial camera with result overlay in video livestream

IDS NXT malibu: AI directly on the camera + compression via ISP + video streaming via RTSP

With IDS NXT malibu, we prove once again that pioneering spirit is firmly anchored in the DNA of IDS. The new camera series is part of the AI system IDS NXT and has some very special features: it is equipped with a special chip from Ambarella that enables compressed video streams (H264) with full HD at high speed (> 25 fps) and allows them to be displayed on end devices via RTSP protocol. This means that there is no need for a PC to carry out evaluations/visualisations.