IDS’ industrial cameras on the high seas

Powerful shrimp sorting system with IDS camera UI-5240RE

With the continuous exhaustion of fishing grounds, many fish species have become endangered. For this reason, the fishing industry is searching for solutions to ensure an environmentally responsible approach. Two companies from the Netherlands have developed a shrimp sorting machine that returns by catch consisting of crabs and young fish quickly and unharmed back into the sea. The sorting system was implemented with our uEye RE GigE in an automation system from an Austrian supplier.

Application

A vacuum system sucks in the catch and distributes it on a conveyor belt. Two IDS GigE cameras, each with resolutions of 1.3 mega pixels, take pictures of the individual objects. The software for the image processing is based on a HALCON script. It identifies shrimps and grades them into three different sizes. This enables 10 to 20 images to be analyzed per second, depending on the speed of the conveyor belt.

A controller receives the relevant image data via an Ethernet connection. Different air nozzles get activated and targeted blasts of air transport the shrimps by size into the appropriate container. Bycatch is ignored by the system and stays on the conveyor belt for less than a minute, which returns it directly back into the sea.

Why the decision was in favor of the uEye RE GigE?

“It’s used on a ship!” points the CEO of the involved engineering company. Together with a machine building company, that specializes in the shrimp fishing industry, he developed a visual scanning device with two UI-5240RE cameras, the most rugged industrial camera with Gigabit Ethernet interface in the IDS-portfolio. The magnesium housing, lens barrels, and lockable connectors comply with all the requirements of the IP 67 protection classes. The GigE uEye industrial camera is splashproofed and can even be operated in other extremely harsh environments.

The visual inspection system takes pictures of the shrimps directly on bord. Up to 300 kilograms of shrimps per hour can be sorted and thrown back into the water alive - an eco-friendly approach.

GigE uEye RE industrial camera: Extremely robust, dustproof, and splashproof

IDS Industriekamera GigE uEye RE