uEye XC camera in front of a mountain of old clothes

Efficient textile recycling with AI and image processing

Intelligent sorting of old clothes

At a glance

  • Industry: textile recycling
  • Camera: USB 3 uEye XC Starter set
  • Task: automatically capture, classify and sort used textiles by garment type and material
  • Challenge: high volumes, material diversity and largely manual sorting make efficient recycling more difficult
  • Solution: DETEX uses AI and two high-resolution uEye XC cameras for object detection and material classification on the conveyor belt
  • Customer benefit: more precise and efficient sorting helps keep more used textiles in the recycling loop

The mountain of old textiles continues to grow in Germany every year. Less than one per cent of this enters a closed recycling loop. Reasons for this include so-called “fast fashion”, which leads to an increasing amount of low-quality textiles, as well as the wide variety of materials, which makes efficient recycling even more difficult. Today, sorting is mostly done manually and is almost impossible to manage given the quantities involved: Of around 1.4 million tonnes, only about 200,000 tonnes are actually checked and allocated. The rest is thermally recycled or exported abroad. Automated processes are therefore a key lever for keeping significantly more used textiles in circulation.

The Recycling Atelier at the Augsburg Institute for Textile Technology (ITA) is tackling this challenge. As a model factory, it maps the entire process of mechanical textile recycling. The focus is on a holistic concept that does not optimise individual sub-processes, but rather takes the entire system into account. This approach led to the development of DETEX – an AI-based system for the automatic sorting of textiles. With the help of artificial intelligence and two high-resolution uEye XC cameras from IDS Imaging Development Systems GmbH, DETEX captures the essential features of the garments and assigns them precisely to specific categories. This makes sorting more accurate and lays the foundation for efficient recycling.

Why is sorting old clothes so important?

Before worn-out trousers, T-shirts or jumpers can be turned into something new, they must first be mechanically processed. The aim of this process is to create entirely new fabrics from the used garments. To achieve this, they are shredded, freed from buttons or zippers, and broken down into individual fibres. Preserving fibre length during this process is crucial to the quality of the recycled material produced. Differences in fabric structure and areal density must also be taken into account during processing. Precise classification into material categories is therefore essential and determines the subsequent handling of the textiles.

Until now, sorting has been done mainly by hand – a time-consuming process that requires a high level of expertise. In other industries, such tasks have long been performed by automated, AI-supported recognition systems. This is precisely where DETEX comes in: The research project is developing and testing AI models designed to make the sorting of used textiles significantly more efficient.

Blue T-shirt on green background, uEye XC camera on movable arm inspects from above
The AI uses a uEye XC camera to determine the type of material used in the textiles.

How does the system work?

DETEX relies on intelligent image processing to automatically recognise and classify textiles. Two high-resolution industrial cameras provide the necessary images by scanning garments as they move along a conveyor belt. Neural networks analyse the images and recognise patterns and structures based on previously learned data. To enable this, they were trained in advance using a large number of sample images, including photographs of various garments as well as close-up images of different fabric types. At least 3,000 samples per clothing category were required. This training data had to be manually categorized beforehand, for example by labelling an image of trousers as “trousers“. On this basis, DETEX can quickly and reliably assign new images to the appropriate textile categories.

For precise analysis, DETEX works with pre-trained neural networks – one model each for classification, object recognition and material identification. Different architectures and scenarios are being tested. This allows different degrees of difficulty and realism to be simulated in order to test how robust the AI models are against folds, overlaps or rotations.

Initially, an object detection model analyses the images captured by the first camera mounted above the conveyor belt. It determines the type of garment, such as a T-shirt, trousers or a dress. The second camera scans the garments again from a height of approximately 5 centimetres, focusing on material properties and the detection of features such as stains or buttons. The identified image sections are cropped and passed on to a second AI model, which classifies the type of material – specifically distinguishing between woven and knitted fabrics. Finally, the analysis results are clearly displayed on a screen.

The left display shows a picture of a blue T-shirt, while the right display shows a close-up of blue fabric.
The analysis results are shown on a display.

Which cameras are used?

For image capture, the Augsburg-based institute relies on uEye XC cameras from IDS, specifically the uEye XC Starter Set. The complete package includes a camera, tripod, cables and a macro lens, providing a ready-to-use solution for the research project. Key factors in the camera selection were its compact design, 13-megapixel sensor and ease of use, as Martin Kohnle, Project Manager for AI & Digitalisation at ITA, explains: “The uEye XC is as easy to use as a webcam, but has been specially developed for industrial applications. It delivers razor-sharp images even with varying object distances or challenging lighting conditions.” In addition, features such as digital zoom, auto white balance and automatic colour correction ensure precise capture of even the finest details. As a genuine industrial camera, it was designed with long-term component availability in mind – an important advantage over conventional consumer webcams.

uEye XC camera – positioned above a blue T-shirt – takes a close-up shot.
Thanks to the digital zoom, auto white balance and automatic colour correction, the camera captures every detail.

The Augsburg-based team relies on the free IDS peak camera software for image processing integration. The Software Development Kit (SDK) provides all necessary programming interfaces and tools for operating and controlling the cameras.

“IDS peak enables straightforward and high-performance integration of our cameras via USB3 Vision. The uniform SDK structure greatly simplifies development, control and image acquisition. This enables us to implement our AI-based image processing workflows more quickly and adapt them flexibly.”

— Martin Kohnle, Project Manager for AI & Digitalisation at ITA —

What’s next?

The textile recycling market is increasingly moving towards data-driven, AI-based processes that require high-quality image data in real time. This increases the requirements for camera quality, synchronisation and API compatibility for the recycling studio. Research focuses in particular on the flexible integration of various sensor technologies into adaptive sorting and analysis systems.

DETEX itself is also set to evolve: What is currently a conveyor-belt-based system will be expanded into a modular, mechanical-robotic overall solution that addresses both recycling and reuse. At its core will be a free-fall system enabling multi-perspective, 360° capture of textiles. In addition, a downstream, two-sided shot by robot-assisted grippers will allow for detailed analysis of further material characteristics. This approach makes it possible to capture a significantly broader range of information and to assign textiles even more precisely to suitable recycling or reuse pathways. Another important step towards a closed recycling loop – supported by industrial image processing.

Institut für Textiltechnik Augsburg gGmbH

Logo Institute for Textile Technology Augsburg (ITA)

The Recycling Atelier at the Institute for Textile Technology Augsburg (ITA) is a model and learning factory for mechanical textile recycling. The team is researching pioneering methods for the circular recycling of textiles. The vision: High-quality recycling instead of landfill and energy recovery.

uEye XC

Model used: uEye XC Starter Kit