Ensenso XR Onboard processing

All-in-one package makes the technology user-friendly

Deep Learning opens up new fields of application for industrial image processing, which previously could only be solved with great effort or not at all. The new, fundamentally different approach to classical image processing causes new challenges for users – a rethink is necessary. IDS therefore presents an all-in-one embedded vision package with which every user can implement AI-based image processing in just a few steps and without programming knowledge, and use it on a camera as an embedded inference system. Deep Learning thus becomes user-friendly.

Computer vision and image processing have become indispensable tools in various fields. Image processing systems are increasingly confronted with a constantly growing variety of products and variants and organic objects such as fruit, vegetables or plants. Conventional approaches with rule-based image processing quickly reach their limits if the image data to be analyzed varies too frequently and the differences are difficult or impossible to describe using algorithms. In such cases, a robust automation is not feasible due to an inflexible set of rules. Even if the task is supposed to be easy for people to solve. As an example, a child is able to recognize a car even if it has never seen the special model before. It is sufficient if the child has seen enough other car models previously.

Through Machine Learning, the ability to make flexible and independent decisions can now also be transferred to image processing systems. Using neural networks and Deep Learning algorithms, we can teach a computer to see objects, recognize them, and draw conclusions from what it has learned. Like a human being, such an "intelligent automation" learns and decides on empirical values.

Differences to classical image processing

The main difference to rule-based image processing is how and by whom image characteristics are identified and how the learned knowledge is represented. With the classical or "symbolic approach" an image processing specialist is responsible for selecting the image features that are decisive and describing them according to certain rules. Many lines of source code are required to specify in detail how to solve a given task. Because the software can only recognize what the rules cover. The subsequent execution takes place within defined limits without any room for interpretation. The actual intellectual achievement therefore lies solely with the image expert.

Machine Learning: teach through examples
Machine Learning: teach through examples

The procedure for working with neural networks is quite different. Their advantage is to learn independently which image characteristics are important in order to draw the right conclusion. We then speak of a "non-symbolic approach", since the knowledge is only implicit and does not allow any insights into the solutions learned. Which characteristics are stored, how they are weighted and which conclusions are drawn is only affected by the quantity and content of the training images. Deep Learning algorithms recognize and analyze the complete image content and relate the recognized characteristics to the "terms" to be learned, depending on the frequency of occurrence. The statistical frequency produces what we call experience during training. Google's artificial intelligence specialist Cassie Kozyrkov describes Machine Leraning as a programming tool at this year's WebSummit 2019 in Lisbon. It allows to teach a machine things by examples rather than by many instructions.

The development of machine vision applications based on AI therefore requires a rethink. It is important to understand that the quality of the results – i.e. the speed and reliability of object detection – depends on what a neural network detects and concludes. Here the knowledge of the respective professional plays a very decisive role, who must provide the necessary data sets for the training with as many different example pictures as possible including the terms to be learned. The responsibility for the classical approach, which lay with an image processing specialist, is taken over by a data specialist in Machine Learning.

Lower entry barrier with easy-to-use tools
Lower entry barrier with easy-to-use tools

Start immediately with the Machine Learning all-in-one package

IDS would like to support the user right from the first steps with the new technology. IDS combines Deep Learning experience and camera technology with a all-in-one inference camera package. This enables every user to start immediately with AI-based image processing. With IDS NXT Experience Kit, IDS lowers the entry barrier and provides easy-to-use tools for creating inference tasks in a few minutes without much prior knowledge and executing them immediately on a camera.

The concept is based on three important components:

  • An easy to use training software for neural networks
  • and an intelligent camera platform
  • including an AI accelerator that executes the neural networks on the hardware side.

All components have been developed directly by IDS and are designed to work together perfectly. This makes it very easy for the user and the overall system very powerful.

The cloud-based training software IDS lighthouse leads step-by-step through data preparation to the training of artificial intelligence in the form of a neural network. The user never gets in contact with any basic tools or has to deal with the installation of development environments. As a web application, IDS lighthouse is immediately ready for use. The user has sufficient storage space and training performance for all his projects in an easy-to-use workflow. Log in, upload training images, label and then train the desired net.

With a few configuration settings, the user specifies the speed and accuracy requirements for his application in simple dialogs. IDS lighthouse then selects the network and sets up the necessary training parameters completely independently. The training results already give the user a good prediction about the quality of the trained intelligence and thus enable quick modification and repetition of the training process. The system is continuously improved and upgraded. Without having to plan for updates and maintenance phases, the latest version of the software is always available to everyone. The user can concentrate completely on solving his application without having to build up the knowledge about learning methods and artificial intelligence himself.

IDS uses supervised learning at IDS lighthouse to train neural networks. The Deep Learning algorithms learn with predefined pairs of inputs and outputs. The teacher – in this case the user – have to provide the correct function value for an input during learning by assigning the correct class to a picture example. The network is trained to be able to make associations independently by making predictions regarding image data in the form of percentages. The higher the value, the more accurate and reliable the prediction.

The seamless interaction of the software with the IDS NXT camera families rio and rome ensures a quick success. Because fully trained neural networks can be uploaded and executed directly and without programming effort on one of these cameras. Thus, the user immediately has a completely working embedded vision system that sees, recognizes and derives results from captured image data. With its digital interfaces, even machines can be controlled directly.

Seamless interaction of soft- and hardware
Seamless interaction of soft- and hardware

Embedded Vision Hybrid System

IDS has developed its own AI core for the FPGA of the intelligent IDS NXT camera platform called "deep ocean core", which executes pre-trained neural networks hardware-accelerated. This turns the full-fledged industrial cameras into high-performance inference cameras that make artificial intelligence useful in industrial environments. Image analysis is performed decentralized, avoiding bandwidth bottlenecks during transmission. Cameras based on the IDS NXT platform can thus keep pace with modern desktop CPUs in terms of accuracy and speed of results – with significantly less space and energy consumption at the same time. The reprogrammability of the FPGA offers additional advantages in terms of future security, low recurring costs and time-to-market.

The perfect adaptation of IDS' own software and hardware allows the user to choose the target inference time before training. IDS lighthouse then ensures optimal training settings while considering the AI core performance of the camera. Thus the user expects no surprises during the subsequent execution of the inference, eliminating the need for time-consuming readjustment and re-training. Once integrated, the IDS NXT system remains 100% compatible and consistent in its behavior for the user. Especially with industrially certified applications this is a significant advantage.

Extendable funtionalty using apps and CNNs
Extendable funtionalty using apps and CNNs

Due to the powerful hardware, the Embedded Vision platform is much more than just an inference camera used to execute neural networks. The feature set of the CPU-FPGA combination will be extendable by the user according to his needs in the next development step using vision apps. Recurring vision tasks can then be set up and changed quickly. Even a completely flexible image processing sequence can then be realized. Captured images are first preprocessed, for example, before a quite simple and fast classification sorts good and bad parts. If errors occur, a much more complex neural network can be reloaded in milliseconds to determine the error class in much more detail and transfer the results to a database. Customized solutions can then be easily implemented using an app development kit. Users can then create their own individual vision apps in just a few steps and install and run them on IDS NXT cameras.

IDS NXT cameras are designed as hybrid systems to enable both pre-processing of image data with classical image processing and feature extraction using neural networks side by side to efficiently run image processing applications on a single device.

Summary

IDS NXT Experience Kit makes Deep Learning meaningful and user-friendly for everyone. IDS presents a hardware-software combination that is perfectly matched to each other. Intelligent detection tasks and automation in many (new) application fields are enormously simplified or made possible for the first time. In just a few steps and without programming knowledge, AI-based image processing solutions can be created and executed. With the IDS lighthouse training software, the manufacturer has knowingly moved into the cloud in order to be able to scale storage space and training performance to user requirements. In addition, no update and maintenance phases need to be scheduled to benefit from continuous improvements. This ensures that the latest version of the software is always ready for every user. The manufacturer also offers an inference starter package with all the necessary components as a first step into AI-based image processing. A camera with power supply and lens as well as a training license for IDS lighthouse – everything you need to get started right away.

Think Inferent!