IDS event-based camera series uEye EVS.

uEye EVS: IDS launches new camera series with event-based sensor

Efficient, loss-free capture of fast movements with reduced data volume

How do you capture small, fast-moving objects as efficiently as possible and without motion blur? How do you analyse movements in general without generating large amounts of data? With the new uEye EVS, IDS Imaging Development Systems GmbH is launching an industrial camera with an event-based vision sensor that has been specially developed to meet these challenges. Instead of a continuous stream of data, it only captures relevant events. Compared to classic image-based systems, the volume of data generated is significantly reduced. The uEye EVS is therefore the ideal solution for applications that require efficiency and precision at high speed, such as optical monitoring of vibrations or high-speed motion analyses.

The ultra-compact USB3 camera visualises the smallest movements in real time and completely loss-free. Thanks to its extremely high dynamic range, it even works in almost complete darkness. This is made possible by the SONY/Prophesee IMX636 event-based vision sensor. In contrast to conventional image sensors, it does not capture every image completely at regular intervals (frames), but only reacts to changes within a scene. It transmits events depending on when and where the brightness in its field of view changes - for each individual sensor pixel. The temporal resolution, i.e. the minimum measurable time difference between two successive changes in brightness, can be less than 100 microseconds. "Event-based cameras achieve a remarkable temporal resolution, making them optimised for highly dynamic scenes. The best conditions for capturing fast object movements without loss of information - comparable to an image-based frame rate of more than 10,000 images per second," explains Patrick Schick - Product Owner 3D & Vision Software. At the same time, the sensor ignores all motionless areas of its field of view and thus generates 10 to 1000 times less data than image-based variants. This saves memory and computing time.

With the "uEye EVS" camera line and the first uEye XCP-E product family, IDS offers event-based sensor technology in an ultra-compact industrial format of just 29 x 29 x 17 millimetres. The fully enclosed die-cast zinc housing with C-mount adapter, the compact size and the screw-on USB Micro-B connector make the camera ideal for a wide range of applications in both industrial and non-industrial areas. Further variants will be added to the product line.

Further information: https://en.ids-imaging.com/ueye-evs-cameras.html

Images (© IDS Imaging Development Systems GmbH)

Illustration of the movement of a "waving cat" - event-based on the left, image-based on the right.
The compact USB3 camera uEye XCP-E visualises the smallest movements in real time and completely loss-free.
uEye XCP-E: IDS industrial camera with event-based sensor.
Thanks to the event-based sensor technology, uEye EVS cameras only capture relevant changes in the image.
Various uEye EVS camera models.
The new event-based camera line uEye EVS from IDS.
IDS, Sabine Terrasi
Sabine Terrasi
Communications Specialist – Corporate & Product

She has been designing company profiles, brochures and case studies for over ten years and has supported corporate topics as well as technical product communication. With her background in strategic B2B communication, she ensures clear messages and well-founded content.

Download
Download Word file and images here. 4,81MB

Contact
Please contact our team, we will be happy to help you.

Press contact
Do you need background information, statements or images for journalistic purposes? The IDS editorial team will be happy to help you.

Newsletter
Stay up to date and subscribe to our newsletter.