IDS NXT camera in use for image analysis

Expert in user-friendly AI vision systems

In application development, there is not only the ONE AI solution. And a particular AI vision system is not always the suitable answer to a problem. The application decides how, what and with what. Simplicity, cost, performance and time belong to the most important and decisive criteria for the use of AI vision technologies. The fact that AI-based methods work completely differently than rule-based approaches is both an advantage and a disadvantage. However, this in turn enables manufacturers like IDS to develop entirely new types of tools for image processing that can be used much more intuitively. With them, human quality requirements can already be transferred to AI-based image processing systems through machine learning in order to optimize and automate processes. Often, not a single line of source code needs to be written in the process, making AI vision suitable for entirely new target groups that no longer need to have programming skills. Companies are no longer necessarily dependent on programmers and image processing experts at this stage.

Despite the intelligent new methods, AI vision remains "image processing". To realize a solution, it has to be integrated into an application, like its rule-based counterpart, and work together with other system components. Any user, with or without prior knowledge of AI, image processing or application programming, must also solve this task. And therein often lies the real challenge of an application. Anyone who selects system components purely on the basis of price, performance and richness of features often has to deal with various service providers and manufacturers in the further stages with regard to interfaces of the different systems. Getting them to work together smoothly in a complete workflow often requires patience, time and a lot of in-house expertise.

IDS therefore relies on components that are optimally matched to each other and can be used by all user groups with the support and experience of one single contact partner. This saves valuable time, expensive development resources and gets the user to his individual solution faster.

An IDS NXT AI camera with IDS lens is screwed to a metal profile and connected via PoE. Other system components, such as vision apps, the web-based block editor and the deep ocean AI accelerator, hover around the camera.
With IDS NXT, many simple image analyses can be implemented from the idea to a fully functional embedded AI vision system without the need for any prior knowledge.

Ready-to-use embedded AI vision systems

Artificial intelligence running directly on intelligent industrial cameras - with the IDS NXT complete vision system, AI vision is easy and cost-effective to use. Individually trained neural networks for object detection, classification or anomaly detection as well as industry-standard interfaces and communication protocols turn the autonomously operating cameras into fully-fledged inference systems. The entire development process from image to finished AI application is covered by easy-to-use tools. The cloud-based AI vision studio IDS lighthouse is used to manage image data sets, train neural networks and create complete image processing sequences as vision apps for IDS NXT cameras.

The IDS NXT ecosystem will be expanded this summer with another fast and easy-to-integrate embedded vision platform. The new IDS NXT malibu reduces inference times by up to twenty times compared to the existing models - which means it can execute neural networks much faster. Machine vision results here are integrated into the live image as overlays in a hardware-accelerated manner and provided as compressed video streams (H.264 or MJPG). This makes it the ideal application focus for process monitoring or for visual assistance systems, which you can see for yourself at automatica in Munich (booth B5.203).

AI vision for everyone

However, a stand-alone camera is not always the most suitable platform for a machine vision application. For various reasons, the use of a PC-based system in conjunction with classic industrial cameras may be necessary or advantageous. Performance, connectivity, flexibility, integration into existing systems, to name but a few. Ultimately, the requirements of the planned application alone determine which advantages of a platform are best suited for implementation. However, as a user, you are often faced with the situation of having to decide between different machine vision components for a particular system - with all their advantages and disadvantages. Unfortunately, since you can't cherry-pick and put together your own, you are often forced to make compromises.

IDS customers have no restriction in their choice of system with AI vision. Neural networks trained in the cloud based AI vision studio IDS lighthouse can be used with standard industrial cameras in PC-based systems in addition to IDS NXT AI cameras. Since version 2.4 of the IDS peak software, IDS AI-Vision can also be used by application developers in their own camera applications. IDS provides virtually a machine vision construction kit with all the tools through which the simplicity of AI-based image evaluation can be used with any IDS camera, i.e. not only those of the IDS NXT product line. This allows AI-based inference to be added to any application already running that uses IDS cameras.

High performance AI vision technology as NO-CODE tool

In addition to the IDS NXT system, which is suitable for rather simple and cost-optimized projects, IDS is also setting the course in the area of "high performance" vision applications to offer everything from a single source as an AI partner. For this reason, the Fraunhofer spin-off DENKweit GmbH and the image processing company IDS Imaging Development Systems GmbH will go common ways in the future. Since the beginning of the year, a cooperation has started between the "thinkers" from Halle an der Saale and the industrial camera manufacturer from Obersulm. Both companies share the common goal of making highly complex technologies as easily accessible and usable as possible. For this reason, the two companies want to exploit their commonalities and the resulting synergies.

With DENKnet, the user gets the perfect complement to the IDS image processing components to open up new application possibilities and realize important competitive advantages. With DENKnet, individual image analysis with leading AI vision technologies and highest performance can be implemented in just a few minutes with as few as 15 training images. DENKnet takes care of the necessary stability, performance and the right choice of technology automatically in the background. Thus, the operation through the no-code tool "DENK VSION AI HUB" is designed to be very simple and intuitive and can be used by anyone without prior knowledge. With the combination of DENKnet image processing and IDS cameras, image processing solutions with highest performance (GPU accelerated) and quality can be realized. The IDS peak SDK ensures a seamless integration of the image processing into the customer application.

Several result images of different DENKnet AI applications show e.g. anomaly and object recognition, good/bad checks, object counting and OCR.
With the leading AI vision technologies of DENKnet, many different image analyses can be implemented with the highest performance in just a few minutes.

Summary

IDS has expanded its AI vision portfolio in a short period of time, providing users with the appropriate component for the required platform for each application. From the low-cost "It's so easy!" full featured embedded vision system for simple applications without PC up to high-end image analysis with PC and industrial cameras, everything is covered. Users benefit from seamless support from the camera to the image-based training of a CNN and integration into their own application.