Portrait of a person in front of an image, captured using an event-based camera.

Event-based imaging in the real world – use cases, integration and outlook

Live session and Q&A with Prophesee and IDS

Event-based cameras respond to changes in the scene rather than capturing full frames. This makes them fast, data-efficient and highly effective in highly dynamic processes. In this live session on the Vision Channel, Thibaut Willeman from Prophesee demonstrates where and how event-based image processing can be integrated into industrial applications. The “Event-based Vision Sensor” (EVS) in our cameras was developed by Sony and Prophesee.

In a discussion between Boris Duché from IDS and Thibaut Willeman, you will learn how IDS and Prophesee are working together on the next generation of event-based image processing systems. The session will also cover how customer feedback is making integration and use easier step by step.

In the Q&A session that follows, you can discuss your application directly with our experts. The session will then be available in the media library.

Contact
Please contact our team, we will be happy to help you.

Newsletter
Stay up to date and subscribe to our newsletter.