Knowledge Base

AI for the food industry

AI for the food industry

FOOD-Lab Interview: Intelligent image processing in food production

IDS NXT cameras with artificial intelligence can solve tasks involving the detection of organic and variant-rich objects. In horticulture or agriculture, for example, they are the eyes of harvesting robots or rose cutters, can control seedlings or identify pests. In the food industry they offer enormous facilitation for quality control and completeness checks. You can read about the various application possibilities of image processing with AI in the food sector in the detailed FOOD-Lab interview:

With our industrial cameras with artificial intelligence, our customers can individually train the neural networks themselves without prior AI knowledge.

— Jan Hartmann —
Picture of one of the three IDS managing directors Jan Hartmann
Jan Hartmann, Managing Director of IDS Imaging Development Systems GmbH
Patrick Schick
Patrick Schick, Product Manager 3D Vision & Imaging Software of IDS Imaging Development Systems GmbH

Schick: Here in Obersulm on the company site, which was recently expanded by the b39 technology center, we have very short distances between the development departments and production. This enables us to react very quickly to customer needs and implement them accordingly.

Hartmann: There is another important characteristic compared to the competition. With our industrial cameras with artificial intelligence, our customers can individually train the neural networks themselves without prior AI knowledge.

FOOD-Lab: What does artificial intelligence mean in your cameras?

Hartmann: It is a relatively new topic because initially there was still a lack of computing power. So far, we have only spoken of algorithms that were developed as specific instructions for solving a problem. Thanks to AI, our cameras can now cope with tasks that previously could not or only very laboriously be solved with rulebased image processing (IP). Artificial intelligence opens up completely new fields of application for camera technology and image processing. It allows image processing with strongly varying objects. For example, when it comes to classifying different types of fruit or identifying defective parts. Describing all the variances that occur with classic image processing would be extremely time-consuming and therefore costly. With artificial intelligence, however, such challenges can be overcome in no time at all. IDS NXT cameras with artificial intelligence can solve tasks that involve capturing organic and varied objects. In horticulture or agriculture, for example, they are the eyes of harvest robots or rose cutters, they can control seedlings or identify pests.

In horticulture or agriculture, IDS NXT cameras with AI can detect organic and strongly varying objects, for example when checking seedlings
In horticulture or agriculture, IDS NXT cameras with AI can detect organic and strongly varying objects, for example when checking seedlings

Hartmann: With IDS NXT we have created a platform for a new generation of vision systems for industrial applications. The philosophy behind it means a paradigm shift: Our goal is no longer to develop just individual components, but to offer complete systems that are easy to use and yet flexible. With such a system, all steps of a vision solution can be implemented, from image acquisition to image analysis and processing to the control of industrial production machines.

Schick: With IDS NXT cameras and the associated cloud-based IDS lighthouse training software, this even works without any programming effort. Users only need knowledge of their images and their evaluation in order to create a neural network. For example, think of apples. No two are alike, they differ in shape and color and can have rotten spots. These deviations make it difficult for sorting and monitoring systems – unlike, for example, in metal production, where every screw is almost identical.

Image processing with AI facilitates the quality inspection of food
Image processing with AI facilitates the quality inspection of food

FOOD-Lab: Where do you see applications in the food industry?

Schick: Think about fish processing. The camera tells the robot how is the fish lying on the belt, where is the back, the caudal fin, etc. in order to be able to process it further. Such and similar questions also arise in the meat industry, when testing the quality of fruit and vegetables and the confectionery described. Another application concerns bakeries, i.e. the detection of bread browning from the outside. It concerns e.g. also the packaging of toast in boxes, where the correct distribution of the packages is important.

IDS NXT cameras with AI make tasks such as control, sorting, allocation and completeness checks easier.
IDS NXT cameras with AI make tasks such as control, sorting, allocation and completeness checks easier.