Particles in motion
Event-based cameras in 3D flow diagnostics
How can the movement of air or water be made visible – in three dimensions? Industrial cameras with event-based sensor technology provide a completely new database for this purpose: They only record what actually changes, enabling precise flow analysis with minimal effort. It becomes particularly exciting when several of these cameras are combined, for example, to track thousands of particles in real time in 3D.
New perspectives for flow diagnostics
The precise analysis of flows, whether air, water or other media, is a key tool in research and development. Until now, expensive high-speed cameras have mostly been used to visualise the movement of individual particles. Although these deliver impressively detailed images, they generate enormous amounts of data that must be stored, transferred and processed at great expense. Even at high frame rates, the results are highly dependent on the correct choice of exposure time, lighting conditions and optical configuration. Without extensive imaging expertise, motion blur, dark image areas or incomplete scanning can quickly occur. This significantly impairs the quality of the measurement data.
A new technology promises to remedy this situation: Event-based cameras do not continuously capture complete images, but only register changes in the field of view – with microsecond precision. This neuromorphic sensor technology drastically reduces the data stream while enabling highly dynamic analysis of movements. It becomes particularly exciting when several of these sensors are combined: This makes it possible for the first time to perform complex 3D flow analyses – cost-effectively, scalable and with unprecedented efficiency. A genuine enabling technology that opens new doors for research institutions and industrial applications.
With multiple perspectives into the third dimension
Flow diagnostics relies on the ability to precisely capture movements – ideally not only in two dimensions, but in three. Event-based cameras offer a completely new approach here. Unlike conventional image sensors, they only detect contrast changes in the field of view – with response times in the sub-millisecond range. The resulting data volume is not only significantly smaller, but also highly relevant. Combined with their high light sensitivity and compact design, this opens up new applications that were previously only possible with very expensive high-speed systems.
It becomes particularly exciting when several event-based cameras are combined with each other. Only by viewing particles from different angles can they be clearly identified in space and their movement reconstructed in three dimensions. Applications such as established particle image velocimetry (PIV) or the visualisation of complex compression shock configurations – for example, between engine blades – benefit enormously from this technology. The reduced data stream even allows real-time evaluation, enabling new concepts for active flow control based on imaging measurement technology to be implemented.
The methodology presented here is based on several years of research into event-based image processing in flow diagnostics, as pursued in particular by the Optical Engine Measurement Technology Department at the DLR Institute of Propulsion Technology in Cologne.
From events to 3D data
A single camera is not sufficient to capture the movement of individual particles in a flow field in three dimensions. Only by combining several perspectives – typically three to four cameras – can the particle positions in space be clearly determined. The cameras are placed in a photogrammetric arrangement so that they capture the same volumetric object from different perspectives with slightly overlapping image areas. The 3D position of the particles can be calculated in space using triangulation based on the corresponding pixels and the known camera positions. The more angles of view are available, the more precise and robust the reconstruction of the particle trajectories becomes.
Precise synchronisation is crucial to ensure that the data from the cameras can be correctly merged later on. The four event-based industrial cameras from IDS used for this purpose offer two particularly helpful interfaces:
- Trigger input: It enables a unique timestamp to be placed in all data streams so that events can be precisely assigned to each other later.
- Hardware inhibit (TDRSTN): This function allows all cameras to be started simultaneously – even if they are operated on different computers.
Once the data has been collected, the real challenge begins: The events of the individual cameras must first be geometrically registered with each other (camera calibration). The particles are then localised in space, either directly from the synchronised events or via a two-stage process in which the particles are first tracked in the individual views and then their movement paths are reconstructed. The positions and time stamps of individual pixel events are accumulated over a defined period of time – i.e. merged in terms of time and space. The result is a kind of "motion trail" in space that shows how particles move within a volume over time.
This form of visualisation is particularly helpful for understanding complex flow patterns: You can see whether particles are moving in trajectories, whether turbulence is occurring, or how shock waves are propagating. Backflows, vortex formation and local changes in velocity can also be visualised in this way. Such qualitative representations are not only of great value for research and teaching, but also for the development and optimisation of technical systems, for example in aerospace, fluid mechanics or microfluidics.
Event-based cameras offer an exciting alternative to traditional high-speed systems. Even though they do not yet achieve extreme temporal resolution, they already enable significantly more cost-effective and simplified flow analysis – making 3D PTV measurements accessible to smaller laboratories and research institutions as well.
Advantages, limitations and challenges
The performance of the system depends, among other things, on the temporal and spatial resolution and the sensor. The Sony IMX636 sensor used offers a temporal precision of approximately 100 microseconds. This allows up to 10,000 particles to be tracked simultaneously at a clock rate of 1 kHz – at 10 kHz, the figure is around 1,000 particles. These figures illustrate the potential, but also the limitations, of the technology: Although a higher resolution would allow for more particles, it would also increase the data stream and processing requirements.
However, event cameras offer a cost-effective alternative to highspeed systems. They generate less data, require less storage space and thus enable even smaller research institutions to access precise motion information for 3D flow analyses, for example. Thanks to their compact design and low energy consumption, EVS cameras are ideal for mobile and autonomous systems due to their minimal peripheral requirements, thus opening up new areas of application.
A particularly innovative aspect is the ability to evaluate flow fields in real time at over 250 fields per second. Each "field" represents a complete snapshot of particle movement within a defined volume. This high temporal density not only allows for precise analysis of dynamic flows, but also provides the basis for adaptive systems. In these the flow can be actively influenced, for example, by controlling flaps, nozzles or other mechanical components. For Dr Christian Willert from DLR, this real-time evaluation is a real milestone in the further development of image-based measurement technology.
Enabling instead of revolution
Event-based vision does not compete with traditional image-based systems – it does not replace them, but rather complements them in a meaningful way. While highspeed cameras continue to demonstrate their strengths in situations where maximum spatial resolution and complete image information are required, event technology offers a new, low-threshold option for efficiently capturing dynamic processes. It makes precise movement analysis accessible – even for laboratories and research institutions with limited budgets or infrastructure.
IDS uEye EVS cameras offer a suitable camera platform for this purpose: compact, energy-efficient and with low peripheral requirements. They enable the creation of scalable multi-camera systems without complex hardware setups and work seamlessly with the Metavision SDK from Prophesee, the manufacturer of the innovative EVS sensor technology. This opens up new fields of application, for example in mobile flow diagnostics, wind tunnel models or even on drones.
The fact that event-based vision can be understood as an enabling technology is also demonstrated by Prophesee's continued involvement in the embedded sector: A specially developed kit allows high-speed event data to be processed directly on a Raspberry Pi 5 with low latency. This makes the technology usable for compact, embedded systems as well – for example in robotics, industrial automation or for autonomous flight platforms. This transforms specialised high-performance technology into a flexible tool for a wide range of new applications.
Further information
- You can read more about event-based flow visualisation in our application story: Event-based flow visualisation.
- Find out more about the uEye EVS cameras: To the camera family
Dipl.-Ing. Heiko Seitz is working at IDS since 2001. After years as a developer in the field of camera software, he now supports technological communication at IDS as Product Marketing Manager. With his experience, he bridges the gap between complex technology and practical knowledge transfer – for example in technical articles, webinars, or lectures.