Application example Machine arms over a colourful blurred background

Line scan mode with one click

Quickly switch to camera configurations such as line scan or long exposure

Benefit from the new "User Set Control" starting with IDS Vision Firmware 1.7 by saving and reloading optimally configured camera settings very easily. Access complete camera parameter sets from the camera memory with just one click. With manufacturer "presets", you also benefit from new camera modes such as line scan and long exposure and thus cover a much wider range of applications with your area scan camera.

Background

Industrial cameras offer many useful operating modes that can be optimally configured for any application by numerous parameters. Once you have found the "optimal" setting, it makes sense to save the configuration. Depending on the application, a camera is operated with different settings or switched between several modes. When switching, parameters no longer have to be re-entered step-by-step, but are available with just a button click. The Techtipp explains the functional enhancements of the new Vision Firmware update and the user set possibilities for your application.

Using User Sets

In two customizable "user sets" you can save complete camera settings and retrieve them at a later time. Because you save the standard and model-related function parameters of an IDS camera, these "user sets" are only compatible with this camera and are therefore stored directly in the persistent camera memory and not in a file. In addition, the firmware provides a fixed "default" setting" for continuous image capture that is compatible with most applications. This preset is also ideal as starting point for your specific user sets.

The user set control is explained using the parameter tree of the IDS Vision Cockpit. These settings can of course be applied in any other GenICam compatible application.

To display all relevant user set control parameters in the IDS Vision Cockpit tree view dialog, enter the following regular expression in the search field: "UserSet|SensorOperationMode".
Select the view scheme "Expert" and change the search field option Search icon. to "Regular expressions".

The search function in the IDS NXT cockpit.

Before you load, edit or save camera parameters via user sets, first select the desired set via the "User Set Selector" node. Loading and saving user sets is only feasible with stopped image acquisition!

GenICam node for "User Set" control.
GenICam node for "User Set" control.

Save configuration

Select "UserSet0" or "UserSet1" and execute "User Set Save" to save all currently set parameters in one of the sets.

Not saved are "DeviceUserID" and the settings of the categories "GigEVision" and "LUTControl"! The Default, Linescan and LongExposure nodes are non-writable presets from the manufacturer and can only be loaded.

Load configuration

You can load all user sets available for your model. Choose the appropriate selector and execute "User Set Load". The Linescan and LongExposure sets also change the camera's operating mode. The active camera operating mode can be queried at any time via the SensorOperationMode node. But this parameter is not writable!

Define the default set

The "User Set Default" node is used to define the default setting that will be loaded when the camera starts. Thus, you can start a camera without software intervention directly in a saved line scan configuration.

Customer-specific user sets 1 and 2 can only be selected if parameter configurations have been saved previously.

Line scan mode

Through the "line scan mode", an IDS Vision area scan camera is also suitable for a multitude of simple applications in web inspection, for example of textiles, paper, rims or silicon wafers.  Simple setup and small system costs provide a cost-effective alternative to an original line scan camera. The biggest advantage of an area scan camera with line scan mode is an easy setup of the desired image scene in basic area scan mode and the possibility to re-adjust it at later time.

Configuring the image geometry for the line scan mode
Configuring the image geometry for the line scan mode

The line scan preset optimizes the camera settings to capture a single sensor line in the center of the image (configurable) to continuously scan moving objects at a high line-frequency. With a color sensor, 2 lines are captured for calculating the color information. The active lines are combined to a complete image before being transferred to the PC. The Width and Height can also be adjusted via parameters.

To display all relevant image geometry parameters in the tree view of the IDS Vision Cockpit, use the following regular expression: ^Width|^Height|^Offset X$|^Offset Y$|Sensor Height

The image geometry can also be adjusted very comfortably via the "Camera Settings" dialog of the IDS Vision Cockpit:

The IDS Vision Cockpit supports dialog-based adjustment of image geometry, camera timing, image parameters and image acquisition.
The IDS Vision Cockpit supports dialog-based adjustment of image geometry, camera timing, image parameters and image acquisition.

Once you have defined the active line position and the image geometry, use the image and line triggers to adjust the acquisition time and speed to the object movement of your application. The line scan mode allows using encoders to start the acquisition of the active line at regular intervals with a line trigger, even at varying object speeds. This avoids distorted images of scanned objects.

Typical applications

Application

Description

Frame Trigger

Line Trigger

Printed web material

Frames can be triggered, for example, by a light barrier. The line signal is controlled by an encoder.

Hardware Trigger (Line0)

Hardware Trigger
(Line2 or Line3)

Non-printed web material

There is no frame sync signal. The line signal is controlled by an encoder.

Freerun

Hardware Trigger
(Line2 or Line3)

Printed web material without speed fluctuations

Frames can be triggered, for example, by a light barrier. There is no signal that triggers a line. The starting and braking behavior of the web cannot be compensated.

Hardware Trigger (Line0)

Freerun
(AcquisitionLineRate is crucial)

Unprinted web material without speed fluctuations

There is neither a frame sync signal nor a signal that triggers the lines. The starting and braking behavior of the web cannot be compensated.

Freerun

Freerun
(AcquisitionLineRate is crucial)

The GPIO (General Purpose Input Output) camera inputs "Line 2 and Line 3" are better suited for line triggering than the optical isolated Line 1 input. Although the external circuitry is not electrically isolated, the inputs have a faster response, which is an advantage when using high line frequencies.

Parameter example

The parameter settings for the typical application "printed web material" could have the following appearance:

UserSetSelector 		= Linescan
Execute >> UserSetLoad
OffsetY         		= 700
Height				= 2000
Width				= 1600
OffsetX				= 240
TriggerSelector 		= Framestart
	TriggerSource 		= Line0
	TriggerActiviation 	= RisingEdge
	TriggerMode 		= On
TriggerSelector 		= LineStart
	TriggerSource 		= Line2
	TriggerActiviation 	= RisingEdge
	TriggerMode 		= On
Execute >> AcquisitionStart

The Linescan preset will be loaded with the UserSetLoad command. The AcquisitionStart command turns the system into ready state to receive trigger signals. A light barrier can start image acquisition, as external trigger source on "Line0". The exposure of the active sensor line (700) is started synchronously to the web speed via "Line2", controlled by a web encoder.

Further applications and trigger possibilities with the use of counters, timers or PWM (pulse width modulation) can be found in our tech tip "Triggering according to the Lego principle".

Also in line scan mode, the acquisition and trigger settings can be comfortably adjusted in the IDS Vision Cockpit.
Also in line scan mode, the acquisition and trigger settings can be comfortably adjusted in the IDS Vision Cockpit.

Long exposure

With a preset it is also very easy to setup a long exposure. The "LongExposure" mode prepares the camera parameters for image acquisitions with exposure times over one second. Long exposure is recommended for all applications with image acquisition in low light conditions. Due to the longer exposure time it is not necessary to increase the gain. This also avoids strong image noise.

The preset "LongExposure" shifts the available exposure time for your recordings to a range between 1 second and a model-dependent maximum of several seconds. Apart from that, you can work in this operating mode with the same parameters as in the "Default" mode.

IDS employee Heiko Seitz
Heiko Seitz
Product Marketing Manager

Dipl.-Ing. Heiko Seitz is working at IDS since 2001. After years as a developer in the field of camera software, he now supports technological communication at IDS as Product Marketing Manager. With his experience, he bridges the gap between complex technology and practical knowledge transfer – for example in technical articles, webinars, or lectures.