Triggering according to the Lego principle
We are all familiar with them. The colourful plastic bricks with the patented stud system, which allows you to combine the bricks in any way you wish and let your imagination run free. The Lego principle is as ingenious as it is simple and has turned out to be a recipe for success. The world of machine vision has made good use of this principle.
Background
As the generic programming interface in the field of machine vision, GenICam standardizes and abstracts every feature of a machine vision camera. The Standard Feature Naming Convention (SFNC) now includes many implementation rules for these vision camera features, thereby describing a colourful building block system for innumerable individual machine vision applications. This multitude of different connection options creates added value to machine vision standardization that has hitherto scarcely been considered. There are many undiscovered possibilities especially when it comes to triggering image acquisition. IDS has therefore equipped its vision cameras with the majority of the standard trigger features to let the user’s imagination run free.
Undiscovered possibilities
Camera trigger signals today are much more than hardware lines, which start an image acquisition in the camera firmware within a matter of microseconds. Thanks to GenICam and the SFNC, trigger signals have become abstract signal definitions with a defined behavior and wide-ranging benefits. The separation of trigger-activating signals (software) from trigger-capable device inputs (hardware) makes the possible applications of triggers all the more varied. Furthermore, image acquisition is no longer restricted to an external source. Counters, timers, generated PWM signals or a software event are also potential signaling devices.
With the release of the Vision Firmware V1.5, numerous features have been added to the trigger configuration of IDS cameras. Thus, countless connection options are available for the trigger sources.
Trigger use cases
Function blocks such as Timer, Counter, PWM or UserOutput can also be used very variably as ‘trigger sources’. This opens up countless possibilities for automating the image acquisition of a vision camera. The following use cases describe some of the many trigger possibilities that can be realised with IDS vision cameras. They are described in such a way that they can be directly modelled with the IDS peak Cockpit using the GenICam Node Tree.
Supported camera models
Not all used trigger parameters, signals or events in the trigger use cases are available for all IDS camera models without restrictions. In the linked document you will find an overview of camera compatibility as well as alternative implementation options for affected models.
Trigger compatibility list for IDS cameras
Non-cyclic image acquisition
Use case: Different types of parts are transported on a conveyor belt. A light barrier triggers image acquisition of the parts to read out barcodes for part identification purposes.
Characteristics
- The trigger signal is a software or hardware trigger, for example.
- Non-cyclic trigger signals occur as a result of different parts and distances.
- Immediately after the trigger signal, acquisition starts with the exposure.
- To produce sharp images, the exposure time is preset to the lighting conditions and speed of the conveyor belt.
- Precisely one image is captured for each trigger signal.
- During the acquisition and readout time, no further trigger signal is accepted.
Parameter Settings
AcquisitionMode = Continuous
ExposureTime = 15000
TriggerSelector = ExposureStart
TriggerMode = On
TriggerSource = Line0
The AcquisitionStart command prepares the system to receive trigger signals:
Acquisition Start
Execute AcquisitionStart
If "Line0" is set as the TriggerSource, external hardware trigger sources can now start the exposure, e.g. using signals from a light barrier or a button.
If "Software" is the TriggerSource, use the software trigger command:
Acquisition
TriggerSource = Software
Execute TriggerSoftware
The AcquisitionStop command ends acquisition mode:
Acquisition Stop
Execute AcquisitionStop
Any acquisitions that have already started are still fully exposed and transferred upon execution of the AcquisitionStop command.
Delayed image acquisition
Use case: In a conveyor system, where the trigger sensor cannot be mounted next to the camera for constructional reasons, image acquisition must be started with a delay. The time delay depends on the conveyor speed.
Characteristics
- The trigger signal is a software or hardware trigger, for example.
- Image acquisition starts the specified exposure time with a delay (TriggerDelay) with respect to the trigger signal.
- The TriggerDelay time can be configured (in microseconds from 0 to approx. 16 sec).
- Precisely one image is captured for each trigger signal.
- The individual trigger signals may occur non-cyclically.
- No further trigger signal is accepted during the TriggerDelay and acquisition.
Parameter Settings
AcquisitionMode = Continuous
ExposureTime = 15000
TriggerSelector = ExposureStart
TriggerMode = On
TriggerSource = Line0
TriggerDelay = 500
With these trigger settings, exposure is only started 500 µs after the Line0 trigger signal occurs.
The TriggerDelay can be used with any other TriggerSelector or TriggerSource.
The AcquisitionStart command prepares the system to receive trigger signals.
Acquisition Start
Execute AcquisitionStart
If "Line0" is set as the TriggerSource, external hardware trigger sources can now start the exposure, e.g. using signals from a light barrier or a button.
The AcquisitionStop command ends acquisition mode:
Acquisition Stop
Execute AcquisitionStop
Any acquisitions that have already started are still fully exposed and transferred upon execution of the AcquisitionStop command.
Scaled triggering
Use case: A print web is captured by an IDS camera in line-scan mode. An encoder specifies the cycle time that will allow you to synchronize acquisition with the machine speed and keep the pixels the same size. However, the encoder frequency is not the same as the line frequency, which means that the cycle time must be reduced with the trigger prescaler.
Characteristics
- The input signal is received via a software or hardware trigger.
- The trigger signal starts the specified exposure time for each image acquisition.
- Precisely one image is captured for each trigger signal.
- Each xth trigger signal can be processed by the TriggerDivider.
The start signal for the ExposureStart is configured so that an image is only captured on Line0 every 4th signal.
Parameter Settings
AcquisitionMode = Continuous
ExposureTime = 15000
TriggerSelector = ExposureStart
TriggerMode = On
TriggerSource = Line0
TriggerDivider = 4
By starting acquisition manually, the system is now prepared to receive trigger signals.
Acquisition Start
Execute AcquisitionStart
If "Line0" is set as the TriggerSource, external hardware trigger sources can now start the exposure, e.g. the print web encoder.
The AcquisitionStop command ends acquisition mode:
Acquisition Stop
Execute AcquisitionStop
Any acquisitions that have already started are still fully exposed and transferred upon execution of the AcquisitionStop command.
Triggering the acquisition period
Use Case: You want to observe a drop falling. When the drop enters the image area, it is detected by a light barrier and image acquisition starts. Images are captured which document the surface movement of the drop as it falls. A second light barrier at the bottom edge of the image ends acquisition as soon as the drop leaves the image area.
Characteristics
- During the active phase of the trigger signal, images are captured continuously.
- The frame rate and exposure time are fixed.
- The number of images captured is determined by the duration of the active signal phase and the configured frame rate.
Acquisition Configuration
AcquisitionMode = Continuous
AcquisitionFrameRate = 30
ExposureTime = 1000
TriggerSelector = AcquisitionStart
TriggerMode = On
TriggerSource = Line0
TriggerActiviation = RisingEdge
TriggerSelector = AcquisitionEnd
TriggerMode = On
TriggerSource = Line0
TriggerActiviation = FallingEdge
The AcquisitionStart command prepares the system to receive trigger signals.
Acquisition Start
Execute AcquisitionStart
If "Line0" is set as the TriggerSource (rising edge), continuous acquisition starts. If the edge of the trigger signal is on "Line0", continuous acquisition ends.
Any acquisitions that have already started are still fully exposed and transferred upon execution of the AcquisitionStop command.
Cyclical triggering
Use Case: You want to document the course of an object’s movement by means of a time-lapse recording. The exposure time is adapted to the specified length of time.
Characteristics
- Cyclical trigger signals can be generated by a timer or by a PWM signal.
- For high-frequency signals (up to 100 kHz), it is better to use a PWM signal.
- For low-frequency signals (e.g. 1 frame per minute), you can use a timer with an optional trigger signal.
- By using an additional controllable signal level (e.g. UserOutput), you can restart a timer at regular intervals.
- The trigger signal starts the specified exposure time for each image acquisition.
- Precisely one image is captured for each trigger signal.
Parameter Settings
AcquisitionMode = Continuous
ExposureTime = 15000
TriggerSelector = ExposureStart
TriggerMode = On
TriggerSource = Timer0Start
TriggerDivider = 6
The Timer0 is configured to run for 10 seconds (10,000,000 µs). If the signal level of UserOutput0 is set to "LevelHigh", Timer0 constantly restarts. In combination with the divider trigger, only the sixth timer start leads to an acquisition.
Timer Settings
TimerSelector = Timer0
TimerDuration = 10000000
TimerTriggerSource = UserOutput0
TimerTriggerActivation = LevelHigh
By starting acquisition manually, the system is now prepared to receive trigger signals. However, acquisition does not start until the timer starts running.
Acquisition Start
Execute AcquisitionStart
If UserOutput0 is now set to True (=LevelHigh), the timer starts and the first frame is captured immediately. It is recommended to first execute the TimerReset command. This ensures that even the first interval is reset to full length.
Timer Start
TimerSelector = Timer0
Execute TimerReset
UserOutputSelector = UserOutput0
UserOutputValue = True
Using these settings, one image is captured every minute until AcquisitionStop is executed or UserOutput0 is set to False (=LevelLow).
Acquisition Stop
UserOutputSelector = UserOutput0
UserOutputValue = False
Execute AcquisitionStop
Any acquisitions that have already started are still fully exposed and transferred upon execution of the AcquisitionStop command.
Triggered exposure time
Use Case: A camera delivers images that are processed and evaluated directly. It is also possible to determine here whether the images are over or under exposed. The exposure time for the next acquisition can then be adapted dynamically using the pulse generator without needing to change the parameters in the camera.
This type of acquisition is also referred to as “level controlled exposure” or “bulb mode”.
Characteristics
- The trigger pulse width determines the exposure time.
- The exposure starts as early as possible after the exposure start trigger begins (in this case: rising edge on Line0).
- The exposure lasts as long as the time specified by the trigger signals.
- The exposure lasts at least as long as is defined in TriggerControlledExposureTimeMin.
- The exposure is terminated at the latest after TriggerControlledExposureTimeMax.
-
Precisely one image is captured for each trigger signal.
Acquisition Configuration
AcquisitionMode = Continuous
TriggerSelector = ExposureStart
TriggerMode = On
TriggerSource = Line0
TriggerActivation = RisingEdge
TriggerSelector = ExposureEnd
TriggerMode = On
TriggerSource = Line0
TriggerActivation = FallingEdge
TriggerControlledExposureTimeMin = 500
TriggerControlledExposureTimeMax = 1000000
Using the parameters TriggerControlledExposureTimeMin or TriggerControlledExposureTimeMax, you restrict the exposure time to a time range that is suitable for your application. This allows you to avoid exposure times that are too short or too long.
The AcquisitionStart command prepares the system to receive trigger signals.
Acquisition Start
Execute AcquisitionStart
If "Line0" is set as the TriggerSource, an external pulse generator can now control the exposure of acquisitions.
The AcquisitionStop command ends acquisition mode:
Acquisition Stop
Execute AcquisitionStop
Any acquisitions that have already started are still fully transferred upon execution of the AcquisitionStop command.
Interleaved image acquisition
A trigger-controlled exposure time can also be “interleaved” (Interleaved Image Acquisition), depending on the sensor of the camera used. The sensor is already lit up during the readout time ready for the next acquisition. This allows maximum frame rates to be achieved. The TriggerControlledExposureTimeMin parameter also determines the degree of interleaving. The following applies:
- The higher the TriggerControlledExposureTimeMin is set, the more interleaving is allowed.
- If TriggerControlledExposureTimeMin is greater than the duration of the readout, the extent of interleaving does not increase further.
Fastest possible counted image sequence
Use Case: A camera captures parts which are transported on a conveyor belt and are to be subject to quality inspections. Since, for technical reasons, there is no option to hold the light source stable, three images are always taken in quick succession with different exposure times. The image with the best exposure is then analyzed.
Characteristics
- Several images are captured in quick succession ("burst") for each trigger signal.
- The trigger signal is a software or a hardware trigger, for example.
- The exposure time is preset.
- The series of images is captured as quickly as the sensor will allow.
- A counter is used as a tool for the counted image sequence, which ends acquisition automatically when the required number of images is reached.
- No further trigger signal is processed while the counter is active.
The parameters for acquisition are configured in such a way that images are captured while the counter is counting, i.e. is “active”. The exposure time must be set beforehand!
Parameter Settings
AcquisitionMode = Continuous
ExposureTime = 15000
TriggerSelector = ExposureStart
TriggerMode = On
TriggerSource = Counter0Active
TriggerActivation = LevelHigh
The counter is triggered by an external hardware signal (Line0). Its end value (Duration) is set to the required number of image series. Counting is based on the ExposureStart event. The start signal (CounterTrigger) also resets the counter at the same time. (Counter Reset).
Counter Settings
CounterSelector = Counter0
CounterTriggerSource = Line0
CounterResetSource = CounterTrigger
CounterEventSource = ExposureStart
CounterDuration = 3
By starting acquisition manually, the system is prepared. However, acquisition does not start until the counter is active.
Acquisition Start
Execute AcquisitionStart
You can now capture series of images using the hardware trigger (Line0). Acquisition stops automatically when the counter reaches the preset end value.
The AcquisitionStop command ends acquisition mode:
Acquisition Stop
Execute AcquisitionStop
Any acquisitions that have already started are still fully exposed and transferred upon execution of the AcquisitionStop command.
Counted image sequence with fixed frame rate
Use Case: A camera is used at a set of traffic lights to record the behavior of drivers upon crossing the stop line while the lights are on red. A series of images with an adapted frame rate allows you to draw conclusions with regard to speed, the braking action or a change of direction. This allows you to differentiate between a driver who accidentally crosses the stop line slowly and then stops and one who commits a real traffic violation and fails to stop.
Characteristics
- A defined number of images are captured for each trigger signal.
- The trigger signal is a software or a hardware trigger, for example.
- The exposure time is preset.
- The image series is captured at a specified frame rate.
- A counter is used as a tool for the counted image sequence, which ends acquisition automatically when the required number of images is reached.
- No further trigger signal is processed while the counter is active.
The parameters for acquisition are configured in such a way that images are captured while the counter is counting, i.e. is “active”. The exposure time and frame rate must be set beforehand!
The hardware trigger (Line0) starts the recording of the image series. This stops automatically when the Counter0 end value is reached.
Parameter Settings
AcquisitionMode = Continuous
AcquisitionFrameRate = 30
ExposureTime = 30000
TriggerSelector = AcquisitionStart
TriggerMode = On
TriggerSource = Line0
TriggerSelector = AcquisitionEnd
TriggerMode = On
TriggerSource = Counter0End
The counter end value (Duration) is set to the required number of image series. Counting is based on the ExposureStart event. The start signal (CounterTrigger) also resets the counter at the same time. (Counter Reset).
Counter Settings
CounterSelector = Counter0
CounterTriggerSource = AcquisitionStart
CounterResetSource = CounterTrigger
CounterEventSource = ExposureStart
CounterDuration = 3
By starting acquisition manually, the system is prepared.
Acquisition Start
Execute AcquisitionStart
A hardware trigger (Line0) starts the image series.
The AcquisitionStop command ends acquisition mode:
Acquisition Stop
Execute AcquisitionStop
Any acquisitions that have already started are still fully exposed and transferred upon execution of the AcquisitionStop command.
Fastest possible time-controlled image sequence
Use Case: You want to examine the impact of a drop on different surfaces. To do so, acquisition is always triggered if a drop falls within the image area. In this case, acquisition is maintained at the maximum frame rate for a specified time in order to document the behavior upon impact.
Characteristics
- Several images are captured in quick succession ("burst") for each trigger signal.
- The trigger signal is a software or a hardware trigger, for example.
- The exposure time is preset.
- The series of images is captured as quickly as the sensor will allow.
- A timer is used as a tool for the image sequence, which ends acquisition automatically when the set time has elapsed.
- No further trigger signal is processed while the timer is active.
Depending on the speed and data quantity of the “burst”, the maximum bandwidth of the data interface may be exceeded! You must therefore check whether a burst such as this can be maintained and, if so, for how long, and how long the intervals between the individual bursts need to be.
The parameters for acquisition are configured in such a way that images are captured while Timer0 is running, i.e. is “active”. In other words, as soon as the sensor is ready again after acquisition, the next acquisition starts immediately.
Acquisition Configuration
AcquisitionMode = Continuous
ExposureTime = 15000
TriggerSelector = ExposureStart
TriggerMode = On
TriggerSource = Timer0Active
TriggerActivation = LevelHigh
The timer is triggered by the rising signal edge of an external hardware signal (Line0). Its duration (TimerDuration) is set to precisely one second (1 s = 1000000 µs).
Timer Configuration
TimerSelector = Timer0
TimerDuration = 1000000
TimerTriggerSource = Line0
TimerTriggerActivation = RisingEdge
By starting acquisition manually, the system is now prepared to receive a trigger signal.
Acquisition Start
Execute AcquisitionStart
You can now capture series of images using the hardware trigger (Line0). Acquisition stops automatically when the timer reaches the preset time.
The AcquisitionStop command ends acquisition mode:
Acquisition Stop
Execute AcquisitionStop
Any acquisitions that have already started are still fully exposed and transferred upon execution of the AcquisitionStop command.
Time-controlled image sequence with fixed frame rate
Use Case: The reaction of test objects is to be analyzed and tested when a specific event occurs, e.g. reaction time, behavior, decisions. To do so, image acquisition starts when an external trigger signal is received. For a predefined time period, images are captured at a suitable frame rate to document the reaction.
Characteristics
- Several images are captured in a specified time.
- The trigger signal is a software or a hardware trigger, for example.
- The exposure time is preset.
- The image series is captured at a specified frame rate.
- A timer is used as a tool for the image sequence, which ends acquisition automatically when the set time has elapsed.
- No further trigger signal is processed while the timer is active.
Continuous acquisition (10 fps) starts with an external trigger signal (Line0) and ends when the Timer0 period that was started in parallel elapses.
Acquisition Configuration
AcquisitionMode = Continuous
ExposureTime = 15000
AcquisitionFrameRate = 10
TriggerSelector = AcquisitionStart
TriggerMode = On
TriggerSource = Line0
TriggerActivation = RisingEdge
TriggerSelector = AcquisitionEnd
TriggerMode = On
TriggerSource = Timer0End
TriggerActivation = RisingEdge
The timer is triggered when image acquisition starts (AcquisitionStart) and is set to precisely one second (1 s = 1000000 µs).
Timer Configuration
TimerSelector = Timer0
TimerDuration = 1000000
TimerTriggerSource = AcquisitionStart
TimerTriggerActivation = RisingEdge
By starting acquisition manually, the system is now prepared to receive a trigger signal.
Acquisition Start
Execute AcquisitionStart
You can now capture series of images using the hardware trigger (Line0). Acquisition stops automatically when the timer reaches the preset time. Each additional hardware trigger starts a new series of images.
The AcquisitionStop command ends acquisition mode:
Acquisition Stop
Execute AcquisitionStop
Any acquisitions that have already started are still fully exposed and transferred upon execution of the AcquisitionStop command.
Trigger tips
The following tips and notes help you to avoid errors and better understand the behavior of the trigger features:
- Indented parameters may occur more than once and may have a different value for each parent node.
- Always set trigger sources that are not required to inactive (“OFF”).
- Any image acquisitions that have already started are always fully exposed and transferred, even if control signals end in the meantime.
- To configure trigger parameters, image acquisition must be stopped (AcquisitionStop)! To subsequently use the configured trigger, image acquisition must be started again (AcquisitionStart)!
- If trigger mode is enabled (TriggerMode = ON), the AcquisitionStart command simply sets image acquisition to "ready". Image acquisition only starts with a defined trigger signal for the configured TriggerSource.
- If images are to be triggered continuously, AcquisitionMode is typically set to continuous. Otherwise, image acquisition ends automatically if one image (Single Frame) or a number of X images (Multi Frame) have been captured.
- You can easily simulate external trigger signals using "UserOutputs".
Simulating an external trigger signal
If you wish to test complex trigger applications and do not have any hardware signals available, you can still simulate a trigger signal. To do so, place a UserOutput on a Line (hardware input) and configure this as the output. You can now use the UserOutput to activate and deactivate the Line, as though a hardware signal were present there.
Example: Simulated hardware trigger on Line2
The ExposureStart trigger is placed on Line2:
Acquisition Configuration
TriggerSource = Line2
Line2 is configured as though it were an output with a signal input from UserOutput0:
Line Configuration
LineSelector = Line2
LineMode = Output
LineSource = UserOutput0
Upon activation of image acquisition, the system is prepared to now receive triggers:
Acquisition Start
Execute AcquisitionStart
Switching UserOutput0 on and off now activates trigger signals on Line2 and triggers your application. The signal is created upon activation of the UserOutputValue.
Simulate a trigger signal
UserOutputSelector = UserOutput0
UserOutputValue = true
UserOutputValue = false
Simply reproduce and test trigger use cases
All trigger examples shown in this article use standardised functions as defined in the GenICam Standard Feature Naming Convention (SFNC). The linked compatibility overview shows which of these functions are supported by which IDS industrial cameras.
With the IDS peak Cockpit, you have a user-friendly tool at your disposal that allows you to try out and test the described use cases via the feature node tree without any programming effort.
Continue reading Tip:
‘Hardware Trigger’ image acquisition mode in the IDS peak online manual
How-To Video Tip:
A practical introduction to these trigger options is shown in our Vision Channel video How-to Trigger Everything: Flexible Image Acquisition with IDS cameras
Dipl.-Ing. Heiko Seitz is working at IDS since 2001. After years as a developer in the field of camera software, he now supports technological communication at IDS as Product Marketing Manager. With his experience, he bridges the gap between complex technology and practical knowledge transfer – for example in technical articles, webinars, or lectures.