IDS peak Cockpit: generic parameters
This video explains how to use the generic parameters dialogue in IDS peak Cockpit to access advanced IDS camera features. Discover how the dialogue provides full access to GenICam-compliant camera settings, helping users configure and manage specialised parameters efficiently.
Learn how to navigate the available tabs, search for parameters, view detailed parameter information and create custom dialogues for frequently used settings. The video also demonstrates how to save customised parameter layouts within workspaces for faster access in future sessions.
Topics covered
- Accessing advanced camera features through the generic parameters dialogue
- Understanding GenICam interface information and camera settings
- Using search and parameter information tools efficiently
- Configuring specialised features such as sequencer controls
- Creating custom parameter dialogues for frequently used settings
- Saving custom parameter layouts as part of a workspace
Video timeline
- 00:00 Introduction to the generic parameters dialogue
- 00:21 Accessing GenICam interface information
- 00:45 Exploring camera-specific settings and advanced features
- 01:28 Searching for the right parameters
- 01:53 Configuring custom parameter dialogues
- 02:25 Recommendation video "IDS peak Cockpit: Workspaces"
- 02:45 Summary
Who should watch
Machine vision engineers, system integrators, automation specialists and IDS camera users who need access to advanced camera features and custom configuration options.
Watch now to see how the generic parameters dialogue can help you unlock advanced IDS camera functionality.