IDS peak Cockpit: setting a persistent IP address for GigE cameras

This video explains how to set a persistent (fixed) IP address on an IDS GigE camera and why this configuration is essential for stable, reliable machine vision setups. You’ll learn the exact steps required to configure your network interface card (NIC) and camera using IDS peak Cockpit.

We walk through IP configuration on a Windows system, including how to select the correct adapter, adjust IPv4 (Internet Protocol version 4) settings, and understand subnet masks. The video also highlights recommended performance settings – such as jumbo frames and receive buffers – and shows how to apply and confirm a persistent IP within IDS peak Cockpit. This guide ensures your IDS GigE camera is correctly set up for consistent operation across reboots and network changes.

Topics covered

  • Learn how to set up persistent IP addresses for one or multiple IDS GigE cameras using a guided workflow.
  • Understand how the camera manager automatically identifies suitable IP addresses and applies them reliably.
  • See how the IDS peak Cockpit simplifies camera and network configuration in just a few steps.

Video timeline

  • 00:00 - Introduction
  • 00:07 - Configuring the network interface card (NIC)
  • 00:46 - Adjusting IPv4 settings and subnet mask
  • 01:20 - Performance tips: jumbo frames & receive buffers
  • 01:32 - More information in the camera user manual, IDS peak user manual
  • 01:50 - IDS peak Cockpit: IP configuration
  • 02:50 - Ready to use the camera

Who should watch

This tutorial is aimed at users who want to configure IP settings for one or more IDS GigE cameras quickly and reliably, with a guided workflow and a clear, graphical interface that leads through all required steps.