Cost reduction in aerospace through additive manufacturing

Cost reduction in aerospace through additive manufacturing

Additive in space

Spacecrafts are developed, tested and fully assembled on Earth and transported in one piece by a launch vehicle to their respective places of operation. Each component must be able to withstand the extreme conditions during the launch phase. In most cases, in addition to complex test procedures, this leads to an oversized structure of the spacecraft components, because in orbit they experience only a fraction of the stresses they must endure during rocket launch. The maximum take-off mass required for transport with the launch vehicle and the volume of satellites, for example, thus cause high space transport costs. At the same time, the rocket is space restricted, which limits the design of the spacecraft from the outset. The search is on for processes that expand the possibilities of future space missions, save resources and reduce costs.

One possible approach is to manufacture spacecraft components directly in orbit using generative manufacturing. Generative technologies enable efficient and agile production of components on site. The AIMIS-FYT team at the Munich University of Applied Sciences is developing and researching an additive manufacturing process for this purpose in which the production of components takes place in zero gravity. The equipment needed for space travel do not have to meet the high launch requirements, but can be tailored precisely to the mission requirements. The process is being researched on parabolic flights in zero gravity - supported by a uEye CP industrial camera from IDS.

For this additive manufacturing process, also called "in-situ manufacturing" (Latin in situ 'in place'), the team developed a 3D printer with an extruder through which a liquid photopolymer can be dispensed. "Our 3D printing process can directly print three-dimensional structures in space using a UV-curing adhesive or potting compound," says Torben Schaefer, press officer of the AIMIS-FYT team, explaining the special feature of this technology. Instead of creating the components layer by layer, as is the case with conventional 3D printers, they are created directly by the three-dimensional movement of the print head.

Successful 3D printing of a "diagonal rod" in weightlessness [Image: AIMIS-FYT]
Successful 3D printing of a "diagonal rod" in weightlessness [Image: AIMIS-FYT]

Through the application of UV light, the resin is freely extruded into space in zero gravity and hardens within a short time. In combination with weightlessness, this enables manufacturing without shape restrictions that normally exist due to gravity on Earth. Typical shape limitations are, for example, long overhangs that are not possible on earth or can only be manufactured with elaborate support structures. In zero gravity, it is even possible to create components without a fixed anchor point, such as a pressure plate.

This production process enables a wide variety of designs, such as printed structures for solar panels or antennas. For example, the production of mirrors for parabolic antennas or the manufacture of truss structures for the mounting of solar generators is conceivable. This should be of particular interest to manufacturers and distributors of small to micro satellites or even entire satellite constellations, who can use it to reduce both their unit costs and the launch costs for transporting their systems into orbit.

The resin is cured by UV radiation [Image: AIMIS-FYT]
The resin is cured by UV radiation [Image: AIMIS-FYT]

In addition, the reduced mass of the spacecraft assembled in orbit saves resources and can increase the lifetime of a mission by taking more fuel on board instead. "For satellites, the fuel is usually the limiting factor; at present, it usually lasts for around 15 years," explains Torben Schaefer.

Application

The most important process of the manufacturing process is the printing process itself. This is essentially made up of 3 main phases:

  1. Extrusion of the resin with the aid of the extruder
  2. The resin emerges from the nozzle in a viscous state in zero gravity
  3. Curing of the resin by the UV LEDs.


The printing of straight rods, connections of rods and the creation of free-form rods are tested. In one case, a conventional printing plate is used as the starting point for printing; in another case, the behaviour of printing, free-floating rods is investigated.

The four basic operations of 3D printing
The four basic operations of 3D printing

The main parameters of the printing process are the extrusion speed of the resin, the UV light intensity, the UV light time and the trajectory, i.e. the movement path of the printer. "In our printing process, precise, pressure-stable and constant delivery of the medium is important. At the same time, the parameters should be kept constant during the entire process," explains Torben Schaefer.

A finished truss structure in zero gravity - detail shot from the IDS camera [Image: AIMIS-FYT]
A finished truss structure in zero gravity - detail shot from the IDS camera [Image: AIMIS-FYT]

The USB 3 camera sponsored by IDS keeps a close eye on the process: It watches the nozzle of the printer in close-up and always moves relative to it. This way, the camera follows the nozzle with every movement and always has it precisely in focus. The image is cropped in such a way that the formation of the rods is captured around 4.5 cm below the nozzle. "The IDS camera hereby provides very important results for the discharge of the resin and its curing. The UV LEDs required for curing produce a strong overexposure, which means that difficult lighting conditions prevail. No problem for the U3-3260CP from the IDS portfolio: with the cost-effective 2.30 MPixel Sony sensor IMX249 (1920 x 1200 px), it sets particularly high standards in terms of light sensitivity and dynamic range. This makes the global shutter CMOS sensor with its 5.86 µm pixels predestined for applications like these, which are supposed to deliver a perfect result even in difficult lighting conditions - in this case, strong brightness due to overexposure.

In order to be able to further analyse the exit behaviour from the nozzle in zero gravity, the process is carried out at a slower speed. The contour of the rod must be precisely captured. "For this, the high frame rate and resolution of the camera are crucial for a high-quality evaluation," explains Torben Schaefer from the AIMIS team. With a frame rate of 47.0 fps, the IDS camera ensures excellent image quality and is extremely low-noise - perfect conditions for its task in space. But the simple integration of the camera also convinced the research team.

“We were able to seamlessly integrate the camera into our C++-based monitoring system with the help of the IDS SDK.”

— Torben Schaefer, press officer of the AIMIS-FYT team —
During the parabolic flight of the esa programme FYT, zero gravity prevails for 20 seconds [pictures AIMIS-FYT]
During the parabolic flight of the esa programme FYT, zero gravity prevails for 20 seconds [pictures AIMIS-FYT]

Software

According to him, this is where all the data from the sensors converge and provide a comprehensive overview of the current status of the printer and the individual print parameters. "We can start and stop the recording of the IDS camera and all other measurements with one click. Since there are only twenty seconds of zero gravity on a parabolic flight and there is a break of around one and a half minutes between two parabolas, we only save the most important information by starting and stopping measurements and recordings in a targeted manner." In addition, a live image of the printing process is displayed on the monitor with the help of the IDS software. "This live feed makes it easier for us to set up and quickly analyse the printhead."

Outlook

The findings from the experiments will be used to further optimise the printing process of the four basic 3D printing operations (straight bar, straight bar with start / stop points, free-form bar as well as connections between bars) and to prove the primary functionality of additive manufacturing in zero gravity. The aim is to test the technology in space, as it offers the chance to drastically reduce the cost of components in space technology. "With the AIMIS-FYT project, we have the opportunity to actively shape the future of space travel," says Michael Kringer, project manager of the AIMIS-FYT team.

The powerful little IDS camera has successfully recommended itself for future missions - on Earth and in space.

AIMIS-FYT

AIMIS-FYT logo

AIMIS-FYT: The acronym AIMIS stands for Additive Manufacturing In Space and is the name of a team of four aerospace engineering students at the Munich University of Applied Sciences. The AIMIS-FYT (Additive Manufacturing in Space - Fly your Thesis) team is taking part in zero-gravity experiments as part of the European Space Agency's (ESA) Fly Your Thesis 2020! campaign. IDS accompanies the team as part of its university sponsorship programme.

uEye CP

Model used: UI-3260CP-M-GL

IDS, Silke von Gemmingen
Silke von Gemmingen
Communications Specialist – Corporate & Product

For over ten years, she has been creating press releases and application reports and designing corporate topics and technical product communication with corresponding expertise. Thanks to her experience in strategic B2B communication, she formulates precise messages and delivers well-founded, technically robust content - always with a focus on authenticity and clarity.
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
Applications
Discover how industrial cameras are shaping the future.