IDS uEye XCP camera with multiple metal locking cylinders

AI image processing for highly reflective components in quality control

When glare obscures the view

At a glance

  • Industry: quality assurance / quality control / access control technology
  • Camera: USB 3 uEye XCP (U3-36P0XCP-M-GL Rev. 1.2)
  • Task: automated inspection of high-gloss metallic components for the finest surface defects
  • Challenge: highly reflective surfaces hinder stable detection of very small defects and require multiple viewing angles
  • Solution: AI-supported inspection system with enclosed test box, coordinated RGBW lighting and high-resolution monochrome imaging
  • Customer benefit: significantly reduced inspection time, reproducible quality control and reliable detection of defects below 0.1 mm

Metallic, highly reflective surfaces are among the most challenging objects to inspect in machine vision applications. Reflections obscure details, defects often only become apparent from certain angles, and the quality of manual visual inspections varies throughout the working day. The Austrian company Danube Dynamics, in collaboration with EVVA, a manufacturer of mechatronic access solutions, demonstrates how these challenges can be managed with an AI-supported testing system. The system captures components placed in an orderly manner in a box in one step, automatically assesses surface defects, and integrates quality control reproducibly into the production process.

Background: Challenging surfaces, high requirements

At EVVA, metallic components undergo several process steps and must meet strict quality specifications. These include, among others, locking cylinders, cylinder cores, and other finely machined or galvanised precision parts from access technology. Mechanical defects such as scratches under 0.1 mm and galvanisation errors must be detected – deficiencies that are often hardly visible to the naked eye.

The central difficulty: Highly reflective surfaces reflect light and may conceal relevant features. For a reliable assessment, multiple viewpoints are often necessary. In practice, this complicates maintaining a consistently high quality of manual inspections. A solution was sought that reliably detects defects, supports employees, and integrates stably into the production process.

Angled metal locking cylinder with a fine surface and EVVA logo
Mechanical locking cylinder with a high-precision metal surface – test object of the AI inspection.

Solution: Closed test box, coordinated lighting, AI

To reliably solve these challenging inspection tasks, an AI-powered inspection system was developed in collaboration with Danube Dynamics. The system captures components arranged in a 400 × 300 mm Eurobox in one step, automatically assesses surface defects, and integrates quality control reproducibly into the production process. Up to 126 components are arranged in the box and are tested in one pass. To create constant conditions despite reflections, a closed test box with customised lighting is employed. Four individually controllable RGBW bars allow for different colours and lighting angles to make various defect patterns visible. The coordinated interplay of lighting, image quality, and AI evaluation was crucial.

Test bench with screen and Eurobox containing metal parts for quality control.
AI-based Inspection System: Arranged components in the Eurobox during optical inspection.

The image capture is performed by a monochrome industrial camera of the type IDS uEye U3-36P0XCP-M-GL Rev. 1.2. It is based on the 19.80 MP sensor AR2020 from onsemi, delivers 5K UHD resolution with 5136 × 3856 pixels, and is suitable for inspecting the finest surface details. The 1/1.8-inch rolling shutter sensor in a 4:3 aspect ratio supports detailed imaging of even the smallest defects. The system is complemented by an IDS lens with a focal length of 8.5 mm (Type 20M11-C08528).

“For us, it was crucial that we could capture many arranged components on a large testing area in one step while still reliably detecting the smallest surface defects. Only the interplay of lighting, high-resolution image capture, and AI evaluation makes this quality control robustly manageable.“

— Edwin Schweiger, Co-Founder and COO at Danube Dynamics —

The camera captures the entire Eurobox in high resolution. The image data obtained in this manner enables the detection of the smallest defects in each individual component using AI subsequently. What is crucial is not only the pixel count but also the repeat accuracy under defined lighting conditions. The monochrome version additionally supports a high-contrast representation of relevant surface features.

“Especially with highly reflective surfaces, it is essential to depict fine differences stably and in detail,“ emphasises Jürgen Hejna, Product Owner 2D Cameras at IDS. “The camera's high sensor resolution and easy integration provide a solid foundation for industrial applications.“

Ease of integration was also a decisive factor for Danube Dynamics. The camera can be integrated into the overall system via a standard interface. This reduces the development effort and ensures stable testing results during ongoing operations.

Measurable benefit

The potential of the solution became evident during the first live deployment: The AI detected deviations that even experienced professionals hardly noticed. Above all, the significantly reduced testing time made the benefit immediately measurable.

The previously manual visual inspection of more than 30 seconds per Eurobox has been reduced to under five seconds. The basis for this consists of four defined lighting scenarios, from which four images per component are generated. The subsequent AI inference occurs with a runtime of approximately 10 milliseconds per cylinder.

At the same time, the testing process has been fully digitised. Testing results are now systematically documented and statistically evaluated. Scrap and deviations that were previously not recorded are now transparently traceable. Manual quality control is therefore not replaced but specifically supported. Employees are relieved, testing processes are reproducible, and quality is measurably integrated into the production process.

Another milestone is the ability to retrain the AI independently. EVVA can integrate new product variants and error patterns into the system by itself. This enhances the future viability of the solution and allows for adjustments to growing requirements without altering the fundamental system structure.

Outlook

The demands for automated quality control are increasing. At the same time, awareness is growing regarding what is possible with coordinated image capture and AI-based evaluation. While standard applications are relatively simple to implement today, this project demonstrates the potential in the inspection of demanding surfaces. It illustrates how even optically challenging, safety-relevant components can be reliably inspected using lighting, high-resolution camera technology, and AI.

Open door with modern door handle and access fittings in the interior.
Open door with electronic locking system as an example of safety-relevant access components.

Danube Dynamics Embedded Solutions GmbH

Danube Logo

Danube Dynamics Embedded Solutions GmbH is a technology company based in Linz, Austria, which has specialised in intelligent embedded system solutions for industry since 2020. The company develops tailor-made solutions at the interface of software, AI and electronics with the aim of driving automation and digitalisation forward in an efficient, secure and future-oriented manner through "AI at the Edge". Today, Danube Dynamics has over 30 customers across Europe and employs a team of more than 15 highly qualified developers and engineers.

EVVA Sicherheitstechnik GmbH

EVVA logo

For over 100 years, EVVA has been synonymous with mechanical and electronic access systems at the highest technical level. What began in 1919 with the founding of the “Invention-Testing-Utilisation-Institution“ (EVVA) is now a central part of the company philosophy: EVVA conducts its own research, develops and produces independently, and realises innovative mechatronic access solutions. As a family-owned business, EVVA is among the most successful companies in the industry internationally: Over 300 patents have been registered; subsidiaries in ten European markets and worldwide distributors ensure international presence.

uEye XCP

Model used: U3-36P0XCP Rev.1.2

IDS, Silke von Gemmingen
Silke von Gemmingen
Communications Specialist – Corporate & Product

For over ten years, she has been creating press releases and application reports and designing corporate topics and technical product communication with corresponding expertise. Thanks to her experience in strategic B2B communication, she formulates precise messages and delivers well-founded, technically robust content - always with a focus on authenticity and clarity.
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
Applications
Discover how industrial cameras are shaping the future.