Measuring timber using two Ensenso stereo 3D cameras

Wood measuring with Ensenso N20 stereo 3D cameras

Wood measuring with Ensenso 3D cameras

The demand for high-quality wood from sustainable forests constantly increases. Ensenso N20 stereo 3D cameras allow the wood industry the chance to save time and money by a prompt and budget-priced classification of round timber. The fully electronic wood measurement provides an early determination of product-relevant wood properties to optimize follow-up production processes. The receiving measurements on the logyard plays a key role in the evaluation and classification of various trunks: the faster and the more precise the measurement data are, the more efficient the process can be done.

Wood measuring with Ensenso N20 stereo 3D cameras saves time and money by quickly measuring and delivering data. By the fully electronic wood measurement, the forester or sawmill owner can easily recognise whether his 150-year-old oak can be used as valuable, solid floor boards. Or if it can only be used as veneer wood because of not directly visible damage such as heart rot or cavities.

Personnel costs and the blend of extremely valuable resource wood can significantly be reduced. Our Ensenso cameras therefore provide both the profit optimisation in the wood industry and the sustainability in forestry.

The timber is measured using two Ensenso stereo 3D cameras
Measuring station with two Ensenso stereo 3D cameras

How does 3D wood measuring work?

“The cameras are located over the trunk in the measurement system and record it at the side,” says Michael Beer, project manager of Jörg Elektronik GmbH. “The trunk is moved through the system or vice versa to measure it.” Depending on the requirements, the measurement is made with up to four Ensenso N20 stereo 3D cameras which are capturing images during the process. These images are analysed and gathered pixel by pixel.

Thus, the distance of each point can be determined based on the calibration level. Parts of the log profile can easily be created simultaneously by this distance value. The profile sections of the individual measurement units are integrated into a single image via high-performance algorithms.

Based on the 3D data generated during the measurement run, log data are being computed that are used for the calculation amongst others. So foresters and sawmill owners may easily determine the value of the trunk due to the identified wood quality and quantity. By the 3D measurement, a quick, accurate and efficient cutting optimisation and therefore effective cost optimization is also being achieved.

Measurement system with two Ensenso stereo 3D cameras
Measuring station with two Ensenso stereo 3D cameras

“We were impressed by the Ensenso N20 stereo 3D camera because of its high accuracy and compact design.”

— Michael Beer, Jörg Elektronik —
3D measurement result
Wood measuring with Ensenso stereo 3D cameras allows users to get a high accuracy during the measurement and a precise determination of the wood's quality.

Outlook

Michael Beer from Jörg Elektronik made the right decision: Thus, the market leader for measurement of round timber extends its portfolio successfully with another future-oriented solution. The forester is happy, because he benefits from the efficient valuation of his 150-year-old oak tree. Now he has more time to care for the young trees in his sustainably managed forest.

Jörg Elektronik GmbH

JE Logo Scanning Technology

The supplier for round wood spots provides the wood industry with complete systems for metrological data collection (with Ensenso cameras), machine control, data collection and office solutions.

Ensenso 3D camera

Model used: Ensenso N20

IDS, Silke von Gemmingen
Silke von Gemmingen
Communications Specialist – Corporate & Product

For over ten years, she has been creating press releases and application reports and designing corporate topics and technical product communication with corresponding expertise. Thanks to her experience in strategic B2B communication, she formulates precise messages and delivers well-founded, technically robust content - always with a focus on authenticity and clarity.
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
Applications
Discover how industrial cameras are shaping the future.