Knowledge Base

Multi-camera system with AI and seamless traceability leaves no chance for product defects

Multi-cell camera tunnel for automated handling

Completely under control

In areas such as high-precision metal processing, accuracy is non-negotiable. This includes the automotive industry and its suppliers, which is in a deep crisis in Germany for a variety of reasons. It is not only trade conflicts, but also a lack of innovation, high costs and poor efficiency that are weakening the German automotive industry. Companies are under enormous pressure not only to reliably deliver products of impeccable quality, but also to reduce their operating costs at the same time. Digital solutions are needed in production to overcome product anomalies and reduce reject rates. The answer: Artificial intelligence in combination with computer vision and linking quality data with production data.

However, the requirements are high: In order to meet the strict quality assurance standards of the automotive industry, even complex component geometries must be inspected at high process speeds - and with maximum precision and process reliability. Variations in detection, insufficient traceability to individual serial numbers or batches and challenges caused by changing environmental conditions can lead to costly errors, production downtime and complaints.

Round aluminium component of an electric motor inside a test cell
Round component geometries with strong reflections must also be inspected with process reliability

VIVALDI Digital Solutions GmbH has developed an exemplary, innovative solution for AI quality inspection in real time. In addition to an edge server with an Intel processor, intelligent image processing plays a key role in the so-called SensorBox. Designed for an automotive supplier and its production site in the Czech Republic, up to 70 USB3 uEye+ XC autofocus cameras from IDS Imaging Development Systems perform automatic visual inspection for surface inspection in several inspection cells.

More than a dozen IDS uEye XC cameras capture the outer surface of a round aluminium component.
Simultaneous image recording ensures a complete inspection and helps to maintain the cycle time

"The IDS cameras integrated into the test cells capture high-resolution images of the surface of aluminium components from German OEMs, in this case an electric motor," says Uwe Siegwart, Managing Director at Vivaldi, explaining the camera's task. The captured images are pre-processed to optimise factors such as exposure, white balance and colour correction. The AI recognises various surface defects such as scratches, pores or dirt. "There are strict requirements at the plant in the Czech Republic. According to the defect catalogue, defects from 0.2 millimetres must be reliably detected. The test time per component must not exceed 36 seconds," says Uwe Siegwart, explaining the stringent guidelines. Up to 2,400 electric motor housings per day are tested 100 per cent automatically with the successfully implemented system.

Why did the AI specialist choose the uEye XC camera from IDS?

"In addition to the interface to the self-developed cam controller and the compact size, the range of functions of the sensors and, of course, the price due to the number of cameras required, also played a role," says Eike Humpert from Vivaldi's Business Development department. "The decisive factor was that the autofocus camera can capture several surfaces at different distances from the camera." This simplifies the testing process enormously and ensures greater efficiency and flexibility. This is a crucial factor when, for example, different component variants need to be tested. With the macro attachment lens, the minimum object distance of the camera can also be shortened very easily.

The 13.10 megapixel CMOS sensor AR1335 from onsemi, with which the compact uEye+ XC is equipped, also scores highly here. The rolling shutter colour sensor (4200 x 3120 px, pixel size 1.1µm) delivers 20.0 images per second and ensures detailed images. "The BSI pixel technology enables the sensor to deliver consistently precise and reliable results, even in changing light conditions," explains Jürgen Hejna, Product Owner 2D cameras at IDS. It is not only the excellent low-light performance and minimal pixel noise that make the sensor particularly suitable for this application. "The 24x digital zoom, combined with auto white balance and precise colour correction, contributes significantly to the success of this demanding test procedure," emphasises Jürgen Hejna. With dimensions of just 32 x 61 x 19 millimetres, the camera is compact, robust despite its light weight and absolutely suitable for industrial use. The 2D camera expert mentions another plus point: "The components used here are characterised by long availability, one of the most important requirements for solutions for the automotive industry."

Simple integration and maximum performance with the help of IDS peak

"To fully utilise the aforementioned advantages of IDS cameras via USB3.0, we rely on IDS peak. The SDK provided by IDS enables us to seamlessly integrate the IDS Vision transport protocols into our code," says Uwe Siegwart, explaining the integration. With the powerful software development kit from IDS, the industrial camera with USB3 Vision could be programmed specifically for this application. "We use a REST API that generates images with IDS peak via the IDS USB3 Vision transport protocol. Thanks to IDS USB3 Vision, we have a bandwidth of 5 Gbit/s or more available via USB3.0 - compared to the alternative with the Video4Linux driver, where the transfer rate via USB2.0 would be limited to 480 Mbit/s," adds Uwe Siegwart. The resulting advantage: higher resolutions and shorter transmission times thanks to the increased bandwidth.

Screen shows a defective component and the menu with the camera settings
The camera settings can be conveniently changed directly in the Vivaldi software thanks to the IDS peak interface

AI-supported analyses and synchronous camera control via edge server

The simultaneous image processing task is complex and the challenges are diverse. Aluminium parts often have very shiny surfaces that reflect light and therefore have a strong influence on images. These reflections make it difficult to reliably recognise defects such as scratches, cold runs, chatter marks or surface irregularities, as they are often obscured or distorted by light reflections. In addition, it is often the case with aluminium parts that untreated surfaces look different every time. Areas where no processing has taken place show different structures and colour nuances, but these should not be confused with genuine defects. AI-based image processing must therefore be able to distinguish precisely between the normal material structure and actual raw areas in surfaces to be processed that are considered defects.

Image processing is also made more demanding by the ambient conditions in production halls. Factors such as air quality, particularly due to a mixture of cooling lubricants, can affect the clarity and sharpness of the images. In addition, there are temperature fluctuations and vibrations caused both by the mechanics in the box itself and by other machines in the vicinity. These vibrations can lead to blurred images or positional deviations, which makes fault detection even more difficult.

Precise coordination of the image processing systems was necessary to meet these challenges. Lighting, camera positioning and image evaluation algorithms have been adapted so that reflections are minimised and material differences are correctly interpreted. At the same time, the system is robust enough to compensate for interference from environmental factors and deliver consistently reliable results. Defective components must be able to be replaced quickly and easily by the customer's own maintenance team.

"Image processing is carried out via an optimised infrastructure. Up to eight cameras can be connected per USB hub, enabling simultaneous recording of several inspection areas. A maximum of two of these USB hubs are connected to a self-developed 'cam controller', which bundles and processes the image signals. Several cam controllers are networked with the edge server. This server not only calculates the AI-supported analyses, but also communicates directly with the system controller, which coordinates the triggering of the cameras and ensures synchronised recording."

Screenshot of the AI PreCheck of the Vivaldi software
"Human-in-the-loop" in practical implementation - the AI PreCheck is evaluated by humans

Step by step to automated final inspection

Many companies are still reluctant to introduce new, AI-supported technologies. Vivaldi's process does not directly replace existing quality control. "In the first 8 to 12 weeks or so, the classic manual final inspection is carried out as before and supported by our vCHECK module," explains Eike Humpert. This means that the final inspector no longer documents the defects manually using tally lists or defect cards, but instead marks them digitally on the individual (detail) images. A digital interface via a touch PC is available at the final control station for this purpose. The final inspector locates the defect on the image and categorises it according to a predefined defect catalogue.

This has two advantages: Firstly, the final inspector is introduced to the digital final inspection step by step and gets used to working hand in hand with Vivaldi. Secondly, the labelled product images with error marking and classification are used to train the AI. In addition, existing product images are used for training, e.g. recognised defective parts from the past, which are documented as part of the complaints process.

"By combining manual and automated surface inspection, we can achieve an error rate of less than one per cent, even with large quantities," emphasises Eike Humpert. At the same time, this approach enables the AI to be continuously trained. The user has constant control over the extent to which the AI checks and controls.

Always in focus: real-time image recognition in combination with storage of information for traceability

With the implementation of the CamBox in combination with high-performance USB3 industrial cameras, a decisive advance in quality assurance has been achieved. This technology enables stable and high-precision component testing - even at extremely high process speeds. The quality of the detections remains constant, without any fluctuations.

A decisive advantage is the reliable detection, even if individual ambient conditions change. Fluctuations in lighting, temperature or other external influences do not affect the test accuracy. Thanks to the ability to analyse several inspection characteristics simultaneously, the efficiency of the inspection processes is significantly increased.

Test cell with electric motor housing in the background, surrounded by numerous IDS cameras
42 uEye XC cameras inspect an electric motor housing

Another outstanding feature is the automatic image storage for each individual serial number, which guarantees complete traceability of the process and quality data. This means that test results can be traced and documented at any time - a decisive factor for quality assurance in one of the most demanding industries in the world. "Humans must continue to have the last word," says Uwe Siegwart. "Everything has to meet the strict QA guidelines of the OEMs. The complete value-added life cycle of each component must be documented in an audit-proof manner. This means which part was on which system when and was tested with which test equipment and which results." The Vivaldi system guarantees all of this:

Four-cell inspection box, in the background an employee at the post-inspection workstation
4-cell CamBox with post-inspection workstation

Benefits at a glance:

  • Stable component testing even at high process speeds
  • Reliable detection without fluctuations
  • Reliable detection despite individual changes in ambient conditions
  • Simultaneous inspection of several inspection characteristics
  • Automatic image storage for complete traceability
  • Easy maintainability of the components
  • Traceability at component level (process and quality data)

"Image processing is a central component for traceability, which is the actual technological centrepiece of the solution, and IDS is the ideal partner for this point. This closes the circle between quality assurance and traceability"

— Uwe Siegwart, CEO at Vivaldi —

"Our technology is flexible and the platform is scalable. It is optimised for state-of-the-art technology and can be seamlessly integrated into a wide range of manufacturing processes," explains Uwe Siegwart. "Thanks to the scalability of the solution, companies from a wide range of industries can adapt their quality control to individual requirements." Intelligent data processing of process and quality data enables sources of error to be recognised at an early stage, leading to continuous process improvement in the core process of manufacturing companies.

"Digitised quality data acquisition in real time and linking with other production parameters not only increases efficiency, but also significantly reduces rejects and rework. Errors are minimised, costs are reduced and production processes are optimised." The system has already paid off in the Czech Republic: The number of complaints per year has been reduced by two thirds and the number of unrecognised surface defects has even been reduced to zero.

Outlook

The market for digital quality control is developing rapidly, particularly due to more favourable camera technology, for example with regard to higher resolutions. Optimised image processing processes and tools also make it possible for real-time analyses to be carried out by end users," states Eike Humpert. "Improved resolution, more compact design and price-optimised cameras are in demand." The portfolio of the industrial camera manufacturer IDS is designed to meet this demand with state-of-the-art technology.

VIVALDI Digital Solutions GmbH

Vivaldi logo

VIVALDI Digital Solutions GmbH develops state-of-the-art solutions for AI-supported quality control based on the latest computer vision and machine learning technologies. The Vivaldi platform ensures that every component fulfils the highest quality and safety standards, guarantees incorruptible precision and high process reliability in surface visual inspection and raises manufacturing processes to a new level.

uEye XC

Model used: U3-36L0XC

IDS, Silke von Gemmingen
Silke von Gemmingen
Communications Specialist – Corporate & Product

For over ten years, she has been creating press releases and application reports and designing corporate topics and technical product communication with corresponding expertise. Thanks to her experience in strategic B2B communication, she formulates precise messages and delivers well-founded, technically robust content - always with a focus on authenticity and clarity.