Intelligent, camera-based tool protection in stamping and forming technology
Evolution in the press shop
Boosting efficiency through digitalisation - almost no branch of industry can evade it. Also operators of press shops are increasingly networking their production. But - regardless of whether it's a single press or press lines - it's not always necessary to replace the entire plant in order to stay up to date. Retrofitting existing lines, true to the principle of "sensible evolution instead of cost-intensive revolution", is often the order of the day. With Visual Die Protection, Schuler Pressen GmbH from Göppingen offers a solution for avoiding expensive die damage and its consequential costs in stamping and forming technology - retrofittable for existing lines. Equipped with industrial cameras from IDS Imaging Development Systems GmbH and intelligent software, the production process can be monitored as required.
Application
The principle of the system is simple: Visual Die Protection (VDP) detects possible causes of die damage in the press shop at an early stage and stops the line in fractions of a second before damage and downtime occur. Different monitoring functions can be set up for the various areas in the press installation space. This way, a wide range of error sources can be covered to prevent unforeseen incidents. The probability of failure is reduced and the safe operation of the systems is ensured.
The control functions range from checking the component position to foreign object detection and in-process inspections to the targeted monitoring of individual tool functions. For example, if a foreign object, such as a scrap of sheet metal from the previous press pass, is detected in the die, the press stops automatically so that the foreign object cannot push into the die surfaces or cause damage.
For this purpose, 2 to 4 cameras per system monitor the tool room of the press or, if desired, other areas of the plant, such as the scrap chutes. At each stroke, the current process is compared with the target state. If the process deviates significantly from the norm, e.g. due to the above-mentioned foreign object in the tool, the system is stopped and damage and its consequential costs are prevented.
In addition, all image and analysis data are available to the customer for complete traceability. For continuous improvement processes, the system simultaneously links image and process data and optimises its settings with the help of intelligent data analyses. It only intervenes in the production process when there is a critical deviation. Visual Die Protection thus ensures greater process reliability of production plants, prevents tool damage, increases plant availability and secures the user's ability to deliver. Especially in just-in-time supply chains, this is a decisive competitive advantage.
The system can be used for a wide range of monitoring tasks, even outside the actual pressing plant. Thanks to the easy retrofitting of existing systems and the wide range of applications, the monitoring functions can be set up in just a few minutes. Accordingly, customers benefit immediately from camera-based tool protection. That also applies to non-Schuler systems. With the help of product data handling, even monitoring of already set-up tools can be loaded and monitored from the first press stroke.
Camera
The image data on which the Schuler system is based is supplied by uEye CP industrial cameras from IDS. CP stands for "Compact Power" and symbolises compact, visual power packs for industrial applications of all kinds. They offer maximum functionality with extensive pixel pre-processing and are perfect for multi-camera systems thanks to the internal 120 MB image memory for buffering image sequences. The GigE cameras with a size of only 29 x 29 x 29 millimetres score particularly well in terms of light sensitivity, dynamic range and colour reproduction. This makes them predestined for applications that need to deliver a perfect result even in low light conditions, such as in quality assurance or automation. "The quality of the image data convinced us. Even under rather unfavourable lighting conditions in press shops, the camera provides perfect source material for our inspection systems," explains Christoph Pölzl - Project Manager in the Digital Solutions division at Schuler Pressen GmbH. For integration, the company used the IDS Camera Manager, a central and convenient tool for managing all uEye industrial cameras.
“The quality of the image data convinced us. Even under rather unfavourable lighting conditions in press shops, the camera provides perfect source material for our inspection systems.”
Outlook
Visual Die Protection has been on the market since 2019 and has since established itself in stamping and forming technology as a reliable visual protective tool. With artificial intelligence and industrial cameras, it provides a clear view in the press shop. "For the future, we expect a continuously growing market," predicts Christoph Pölzl. In addition to process and tool monitoring, further applications in the area of in-process quality monitoring are added. In addition, the diagnostic tools for linking image and process data are also constantly being expanded. So the evolution continues and perhaps in the end it will lead to a small revolution?
Schuler
Schuler offers customer-specific cutting-edge technology in all areas of forming technology - from networked presses to press shop planning. In addition to presses, the product portfolio also includes automation and software solutions, tools, process know-how and service for the entire metalworking industry. The company is part of the international technology Group ANDRITZ.
She has been designing company profiles, brochures and case studies for over ten years and has supported corporate topics as well as technical product communication. With her background in strategic B2B communication, she ensures clear messages and well-founded content.