Knowledge Base

Camera-based precision sorting helps professionalise farm shops and family-run farms

IDS industrial camera monitors potato sorting at the farmsort facility

Smart farming kept on track

At a glance

  • Industry: agriculture / smart farming / food processing / potato sorting
  • Camera: USB 3 uEye CP (U3-3270CP Rev. 2.2)
  • Task: sort unwashed and washed potatoes by size and quality into multiple fractions in a continuous process
  • Challenge: rising quality requirements, labour shortages and the need for reproducible sorting results despite soil, foreign material and difficult harvest conditions
  • Solution: Farmsort.one combines a fully electric track system with a 1.5-metre inspection section and two or three cameras for repeated optical inspection and targeted rejection
  • Customer benefit: up to five fractions, throughput of 1.4 to 1.7 tonnes per hour under practical conditions and for more than half of the farms no manual re-sorting step anymore

Rising quality requirements and labour shortages are forcing agricultural businesses to modernise their sorting processes. Those seeking to ensure product quality while reducing the burden on staff need more than a simple pass/fail separation system. What is required is multi-grade sorting that reliably classifies produce by both size and quality and has proven itself in continuous operation. This is exactly where the Farmsort.one optical sorting machine from the German company schmiede.one comes in. It brings industrial inspection principles to small and medium-sized agricultural businesses, combining size grading and quality inspection in a single pass. In most cases, it eliminates the need for manual re-sorting altogether.

Structured inspection along a defined inspection path

The core of the system concept is a 1.5‑metre inspection path. Along this track, each potato is visually inspected several times. Depending on the configuration, two or three industrial cameras from IDS Imaging Development Systems monitor the continuous product flow from different angles. Unlike systems that inspect each tuber from all sides at a single inspection station, the assessment does not rely on every individual object rotating freely. Instead, quality is evaluated directly within the process, based on repeated inspections, redundancy and controlled product handling. This enables the system to deliver reproducible results even when foreign material or adhering soil is present.

“We did not want a spot assessment like those used in many conventional systems on the market, but rather a controlled inspection over a defined distance,” explains Jan Kiwitt, Project Manager at schmiede.one. “The combination of a guided conveyor system and multiple inspections enables reliable detection of quality characteristics while maintaining a consistent throughput.”

Farmsort.one is integrated into an existing potato sorting line with a defined material flow.
Farmsort.one as part of an existing sorting line: The 1.5‑metre inspection path enables reproducible quality assessment within the flow of goods.

Electric conveyor‑based sorting for stable processes

Farmsort.one sorts both unwashed and washed potatoes into up to five grades at throughput rates of up to two tonnes per hour. At the core of the system is a fully electric conveyor-based track system, a concept previously used primarily in large-scale industrial operations. Compared with pneumatic sorting mechanisms, it offers more precise product handling, lower wear and tear, and reduced energy consumption. The controlled guidance of the produce forms the basis for consistent sorting results, even when processing unwashed potatoes, foreign material or crops harvested under challenging conditions, where free-flowing systems can lose accuracy. At the same time, it enables continuous operation regardless of labour availability.

Camera technology as an objective measure of quality

For visual inspection, schmiede.one relies on industrial cameras from IDS. They capture each potato multiple times along the 1.5-metre inspection section, enabling objective quality assessment directly within the sorting process. For compact integration into existing sorting lines, USB3 Vision industrial cameras are used. Short transmission paths, straightforward integration and reliable image transfer ensure consistent inspection performance throughout the entire inspection section.

Farmsort.one with integrated IDS camera for potato sorting
USB3 uEye CP cameras from IDS handle the classification of the potatoes

Depending on the specific configuration of the system, two to three IDS U3-3270CP Rev. 2.2 USB 3.0 Vision cameras are used. One camera classifies the objects and detects both foreign objects, such as stones, and small defects on the tubers, such as wireworm holes. Another camera tracks every single object along the conveyor belt. When used in conjunction with a rotary encoder, the position of each tuber can be determined with precision, enabling damaged produce or produce that does not meet specifications to be selectively removed.

Integration is carried out using the IDS peak SDK, which supports reproducible parameterisation, correct camera mounting and precise focus adjustment. “In line-integrated sorting systems, reliability and integration security are key factors, alongside image quality,” emphasises Jürgen Hejna, Product Manager for 2D Machine Vision at IDS. “Reliable interfaces, long-term availability and reproducible camera settings are crucial for low-maintenance continuous operation.”

Farmsort.one’s inspection zone with cameras for sorting potatoes.
A look inside the Farmsort.one inspection zone: Several cameras scan each tuber along the defined inspection path.

Size and quality grading in a single pass

Rather than simply distinguishing between “good” and “bad” produce, Farmsort.one sorts potatoes by both size and quality in a single pass into up to five grades. Defective potatoes are removed via the first outlet, oversized potatoes via the second, while Grade A produce remains in the main product stream. This results in market-ready produce straight from the sorter, eliminating the manual re-sorting step typically required when using systems that only separate defects. Under real-world operating conditions, many farms achieve throughput rates of 1.4 to 1.7 tonnes per hour without compromising sorting accuracy. As many as 73 per cent of users have eliminated manual re-sorting altogether, significantly reducing their reliance on sorting personnel.

The Farmsort.one system sorts potatoes on an existing sorting line.
Combined size and quality grading: Farmsort.one separates defective, surplus and grade A produce in a single pass.

The system can be easily controlled via remote monitoring. The video shows how the goods are inspected on all sides and then sorted: The first discharge outlet removes stones, while the second is allocated to Grade B produce.

Scalable line concept with long-term investment security

The system has been designed with a modular architecture. Growers can start with a smaller configuration and later expand the system with additional sorting outlets or extra cameras. The line control system is designed for flexibility and supports both 24 V signals and FlowControl. An optional remote monitoring capability allows sorting parameters to be adjusted and optimised remotely.

Farmsort.one is a solution developed within the Grimme Group and is already in use at more than 50 farms. Service and sales are supported by an established network, helping to ensure the system’s technical availability during season-critical continuous operation.

Outlook

Additional methods for improving defect detection are being investigated for future applications. These include monocular depth analysis and multispectral inspection methods in the NIR and SWIR ranges. The aim is to reliably record further quality characteristics and to supplement visual sorting with additional objective criteria.

Industrial cameras and Software from IDS provide the technical foundation for stable, repeatable inspection and enable the integration of camera-based quality assessment into compact sorting lines.

schmiede.one GmbH & Co. KG

Schmiede.one logo

schmiede.one is the Grimme Group’s innovation lab. With an interdisciplinary team, the company develops new automation solutions and digital products to make agriculture more efficient, local and sustainable.

uEye CP

Model used: U3-3270CP Rev.2.2

IDS, Silke von Gemmingen
Silke von Gemmingen
Communications Specialist – Corporate & Product

For over ten years, she has been creating press releases and application reports and designing corporate topics and technical product communication with corresponding expertise. Thanks to her experience in strategic B2B communication, she formulates precise messages and delivers well-founded, technically robust content - always with a focus on authenticity and clarity.