Easy uEye+ camera integration in HALCON using IDS peak

This video explains how to seamlessly integrate IDS uEye+ cameras into HALCON using IDS peak, covering both USB3 vision and GigE vision setups. It demonstrates how to select the correct acquisition interfaces, install the right drivers, and enable advanced IDS‑specific features such as network reconnect.

You’ll learn how GenICam producers and consumers work together, how to access standard and vendor‑specific parameters, and how to switch between different transport layers. The video also provides clear, practical examples using live camera connections, showing how IDS peak enhances functionality, stability and workflow efficiency in HALCON.

Topics covered

  • How to set up USB3 vision and GigE vision uEye+ cameras in HALCON
  • Installing and selecting the correct GenICam producers and drivers
  • Using IDS peak to enable features such as network reconnect
  • Understanding transport layers, filter drivers and acquisition interfaces
  • Accessing standard and IDS‑specific GenICam parameters
  • Benefits of IDS peak integration for industrial vision applications

Video timeline

  • 00:00 - Explanation of the setup: hardware & software
  • 01:31 - New feature of IDS peak: reconnect
  • 05:57 - Software components are needed
  • 09:30 - HALCON software
  • 12:57 - Step-by-step explanation with HALCON
  • 18:37 - Step-by-step explanation with IDS software
  • 27:13 - Why should I use the IDS producers?

Who should watch

Perfect for vision engineers, automation specialists, software developers and system integrators working with HALCON and IDS uEye+ cameras.

Watch now to master smooth camera integration in HALCON.