Knowledge Base

Automatic photo portal for the documentation of intralogistics processes

Automatic photo portal for the documentation of intralogistics processes

Drive through control

Due to digitalisation in Industry 4.0, internal logistics is subject to constant change. Internal traceability, i.e. the tracking of goods in the warehouse or production facility, is increasingly playing a key role.  Manufacturers and consumers are placing more and more emphasis on the safety and quality of products. Costly and image-damaging complaints must therefore be avoided. Automation systems can help to optimise goods control here and at the same time facilitate and accelerate the work of the operators - saving time and costs.

Application

The P.Portal is used at Schnellecke to inspect containers with components. For the purpose of documentation and proof in the event of complaints, the filled containers must be photographed. Up to now, employees with digital cameras have taken over this part manually - now four cameras from the uEye CP family each take photos of the corresponding containers. Thanks to a trigger sensor, this happens with repeated accuracy and completely automatically. The PC-based multi-camera system displays and simultaneously stores the image data. The cameras are mounted on a bridge-like construction under which the containers to be documented are passed. Triggered by a distance sensor, these containers are automatically photographed from 4 sides (front/rear/left/right) as they pass through.

In principle, the camera positions are freely selectable, in this case they are to the left and right of the portal. Two lateral extensions of the portal ensure that all pictures can be taken at the same time. The optional Smart Light module enables intelligent light control for the image capture process, actively saving energy costs.

Photo portal with freely selectable camera positions
Photo portal with freely selectable camera positions
USB3 Vision industrial cameras from IDS reliably detect passing containers even at high train speeds.
USB3 Vision industrial cameras from IDS reliably detect passing containers even at high train speeds.

For Sebastian Pose, Managing Director of Pose Automation, important selection criteria for the camera to equip the system were therefore resolution, speed and light sensitivity. In this standardised application, the model U3-3890CP is used. This USB3 vision camera integrated for Schnellecke is predestined for tasks that require a perfect result even with very short exposure times. It features a high-resolution 12.00 MPixel sensor from the Sony STARVIS range, which boasts exceptional light sensitivity and low noise thanks to the sensor's BSI ("back-side illumination") technology. The uEye+ camera also works with extensive pixel pre-processing and has an internal 120 MB image memory for buffering image sequences - a good choice for multi-camera systems such as the P.Portal.

"Basically, the traceability solution P.Portal is designed for the flexible use of different IDS camera models. This enables us to offer our customers a wide range of economic applications. All in all, IDS cameras are characterised by their robustness and particularly easy integration into our systems. The integration is done with the help of the convenient IDS peak software development kit," explains Sebastian Pose.

Software

With the help of software developed by Pose Automation, the images are stored in the client's system with date and time in real time. "What was important to us in the development of the software as well as the overall system was the high degree of automation of the photography process. In addition, P.Portal offers face pixelation with deep-learning technology and is thus DGSVO-compliant," Sebastian Pose explains. In addition, modular extensions are possible, such as the "Smart Light" green technology used here, with which uniform lighting for a passageway switches on and off automatically. Further modules, such as "Code Reading", "Booking Live", "Smart Recording" complete the offer

Each container taken from four sides is displayed in real time on the monitor.
Each container taken from four sides is displayed in real time on the monitor.

The advantages of the system are obvious:

  • Clarity in the event of a complaint: the photographic material can be used to quickly and easily determine whether the damage was already present at the time of handover. This saves time and unnecessary expenses.
  • Complete documentation: The P.Portal photographs the condition upon handover. The logistics process is recorded seamlessly by the cameras.
  • Product and order traceability: Optionally, packaging labels with bar, DMC and QR codes can be automatically read and linked - even with the customer's own booking system.
  • Time neutral: The entire photography process does not take any additional time

Outlook

The quality of products must be right - always and everywhere. The scalable quality assurance solution P.Portal analyses and documents the condition of goods and products - not only during incoming or outgoing goods inspection, but also during ongoing production. There is potential everywhere where intralogistics processes can be automated with the help of image processing. Using the right solution helps companies - regardless of the industry - to further develop their processes and improve their own results.

Schnellecke Logistics SE

Schnellecke logo

The Schnellecke Group is an internationally operating family business that offers a variety of logistics services. With its three divisions Logistics, Transport and Production, Schnellecke covers essential parts of the supply chain for companies all over the world. The company develops overall concepts that range from transport and warehousing to pre-assembly and value-added services to the sequential production of individual parts and modules and container-compatible packaging.

System integrator: Pose Automation GmbH

Logo of Pose Automation GmbH

IDS Solutionpartner Pose Automation GmbH develops high-performance measuring and testing systems for the industrial environment.

uEye CP

Model used: U3-3890CP

IDS, Silke von Gemmingen
Silke von Gemmingen
Communications Specialist – Corporate & Product

For over ten years, she has been creating press releases and application reports and designing corporate topics and technical product communication with corresponding expertise. Thanks to her experience in strategic B2B communication, she formulates precise messages and delivers well-founded, technically robust content - always with a focus on authenticity and clarity.