uEye XLS board-level camera, in front of it a notice that there is a new 20 MP sensor

Tiny, cost-effective board-level cameras now available with high-resolution 20 MP sensor

The new uEye+ XLS cameras with onsemi AR2020 provide impressive 5K UHD resolution

Small camera equals low resolution? This formula is obviously nonsense. However, the fact that the uEye+ XLS models measuring just 29 x 29 x 7 mm now feature a brand-new 20 MP sensor from onsemi with 5K UHD resolution and exceptional image quality is certainly something to be proud of.