More choice: Further uEye+ CP models

onsemi sensors from 0.5 to 18 MP for the uEye+ CP in development

The uEye CP series stands for "Compact Power" and is the small powerhouse for industrial applications of all kinds. Their magnesium housing measures just 29 x 29 x 29 mm, making them a popular choice especially for space-critical applications. You will soon have even more options as we are now implementing the successful onsemi sensors PYTHON 500, 1300, 2000, 5000 as well as the AR1820HS in our USB3 Vision Standard-compatible CP models from the uEye+ product line. Series production is in preparation and is expected to start soon.